Hi,
Im trying to use the 8168 EVM as a PCI E Endpoint but boot from the SD Card.
Im using the Sprectrum Digital EVM (ASSY 512870 REV B).
This is my observation . If I keep the SW3 in the standard/default setting (SD Card Boot Mode) , and disable the Kernel PCI functionality as mentioned in the 81xx PCI Express Endpoint User Guide, the PCIE link does not come up on the PCI E Switch.
However if I set the SW3 in the PCIE Boot Mode as mentioned in the 81xx PCI Express Endpoint Boot Driver User guide, the PCI E Link comes up on the switch..(but its waiting for the boot from PCI as expected)
Is there some SW3 setting that I need to do to enable SD Boot but PCI-E as an endpoint .
If I keep the PCI option in the kernel and have the SW3 in SD card boot mode, then it comes up as a RC and the PCI E link comes up just fine
Thanks
Jayant Jain