Hi,
My customer is trying to connect 1X PCIe video card on DM8168 EVM however nothing is listed under /sys/bus/pci/devices. However, they do see these messages below on console during boot up. Has this been tested before?
ti81xx_pcie: Invoking PCI BIOS...
ti81xx_pcie: Setting up Host Controller...
ti81xx_pcie: Register base mapped @0xd0820000
ti81xx_pcie: Starting PCI scan...
PCI: bus0: Fast back to back transfers enabled
As per the wiki page - http://processors.wiki.ti.com/index.php/DM81xx_AM38xx_PCI_Express_Root_Complex_Driver_User_Guide#Troubleshooting, my understanding is we need to ensure SSC is not used on 1X PCIe video card and reference clock is set to 100MHz. I am assuming our EVM uses 100MHz reference clock with no SSC. Is my understanding correct here?
The customer is using latest EZSDK PSP downloadable from link below-http://software-dl.ti.com/dsps/dsps_public_sw/ezsdk/latest/index_FDS.html. They are using default kernel with no changes as understanding RC mode on PCIe is enabled by default.
Thanks,
Prateek