This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS243EVM: can't connect

Part Number: TMDS243EVM
Other Parts Discussed in Thread: AM2434

I can power up my 243EVM.  All LEDs except LD2 are lit.  I do measure 0.85V at TP8, however.

When I run QuickStart demo, the tool loads the FLASH, and then while attempting to program the core, I get a message:  COM23:230400  Error configuring Debug Server: error=Failed to connecto to AM2434_ALV device: Please unplug your AM2434_ALV, then plug it back in and try again

I also get an error message that the debug server can't connect.

I've tried unplugging/replugging the USB JTAG and UART ports, I've adjusted USB COM port settings, I've tried power cycling, and still, can't get ast the error message to run the quickstart demo.

WHat's wrong?