Hi all,
I am currently working on a project the requires the use of 4 of the GPIO pins on my c5505.
I thought a good place to start was with the example code from code.google.com/p/c5505-ezdsp. So I downloaded the example there [GPIO_test1.zip] and tried to start it but it has not worked. Is there something simple that I'm missing in order to get it to work, that was not put in the example code?
I can get the CLKOUT signal and a signal from the headphone jacks so I don't think my method of reading it is wrong. I have checked the manuals and I follow the code fine, I just get nothing out of the IO.
Hope someone out there can help with this problem! Or else has another example I can download and test with.
Cheers
Daniel