SPRS582B says that these pins are connected to CVDD. Should I connect these pins to CVDD on the PCB? Or they may are left unconnected because already connected to CVDD inside the DSP? In C6457 evaluation boards, for example, these pins are connected to CVDD through zero Ohm resistors.