Part Number: AM6442
Hi Champs,
There are some SBL examples inside the MCU+ SDK. Is any of them in SMP or AMP mode? How can I know?
Regards,
Kien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kien,
The SBL examples are not supposed to be SMP or AMP, these are NORTOS examples running on the R5F0-0 core.
SMP and AMP mode of operation for freertos kernel is only supported for A53 core and these applications can be loaded via SBL, and we do have examples for both of these in the SDK, for example the Hello World example is supported for both SMP and AMP mode: AM64x MCU+ SDK: Hello World Project
Best Regards,
Meet.