This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS243EVM: Loading Elf file with Lauterbach to RAM

Part Number: TMDS243EVM

The firmware of the two cores, R_0_0 and R_01, was previously written to the flash memory.
We are using Lauterbach in "Attach" mode. I can debug the system.
When I load an .elf or .out file in to RAM with data.load  then set Program Counter to main() . 

The error happens at :  bl 0x700D1420 ; System_init. After executing this directive I receive an undefined Instruction intterupt .

  • Hi Ralf

    The support team here has limited experience with Lauterbach tools. 

    It would be best for you to reach out to Lauterbach for support on this.  

    Feel free to ping us, if you do not get the required support from them, I will see if there is anyone beyond our team that can give some pointers. 

    Regards

    Mukul