Other Parts Discussed in Thread: TWL6040
Hi,
I want interface the MIC with Audio Codec (twl6040), here i am using RL=2.2kohm, and C=100nF and supply voltage=2V. also i mapped registers as given below..i am not getting any signal across the output teminal.... please suggest me what changes i need to take...
| Description | D7 | D6 | D5 | D4 | D3 | D2 | D1 | D0 | Value in Register (H) |
| MICLCTL register | X | X | X | 0 | 1 | 1 | 1 | 1 | OF |
| MICRCTL register | X | X | X | 0 | 1 | 1 | 1 | 1 | OF |
| MICGAIN register | 0 | 0 | 1 | 0 | 0 | 1 | 0 | 0 | 24 |
| AMICBCTL register | 0 | 0 | 0 | 1 | 1 | 0 | 1 | 1 |
1B |
Regards,
Venkat