Other Parts Discussed in Thread: AM1808, PMP
Hi all,
We are using AM1808 based EVM. We have SATA support on our EVM. I have made the following the changes in the kernel configuration for SATA support.
Device Drivers --->
<*> Serial ATA and Parallel ATA drivers --->
[*] SATA Port Multiplier support
<*> AHCI SATA support
Then i got the following messages while booting,
ahci ahci: forcing PORTS_IMPL to 0x1
ahci ahci: AHCI 0001.0100 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
ahci ahci: flags: ncq sntf pm led clo only pmp pio slum part ccc
scsi0 : ahci
ata1: SATA max UDMA/133 irq 67
But after sometime i got,
ata1: SATA link down (SStatus 0 SControl 300)
This is the first time iam working with SATA on our EVM. Can anybody help me to solve this problem...
Thanks in advance,
Vivek