This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DMM tiler usable for subframe extraction via DMA

Hi All,

I need to extract an rectangular subframe from a larger frame and send that subframe out as an ethernet packet. Since the EMAC has dedicated DMA, I cannot use the EDMA to do the subframe extraction. I also want to prevent an extra QDMA transfer to extract the subframes before sending them out.

I am already using the DMM LUT in page mode to create "virtual copies" of some RAM pages, that's working fine. Now I was wondering if I could set up the TILER in 32 bit mode so that I can perform a linear DMA that would fetch integers from RAM in the following fashion:

Given an array of integers

0000,0001,0002,0003,0004,0005,0006,0007,0008,0009,000A,000B,000C,000E,000F,

0010,0011,0012,0013,0014,0015,0016,0017,0018,0019,001A,001B,001C,001E,001F,

0020,0021,0022,0023,0024,0025,0026,0027,0028,0029,002A,002B,002C,002E,002F,

0030,0031,0032,0033,0034,0035,0036,0037,0038,0039,003A,003B,003C,003E,003F,

I want for example extract and DMA out

0002,0003,0004,0005,

0012,0013,0014,0015,

0022,0023,0024,0025,

0032,0033,0034,0035,

So these offsets should appear on linear increasing addresses in the TILER view.  Would this be possible? How would I setup the TILER for this behavior?

Thanks,

Stephan