This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to get SGX OpenGL working on BeagleBone (AM3359)



Hello, I'm trying to run the SGX demos included with the TI Sitara SDK 05_03_02_00  from 12/2011. The demos all error with 
"PVRShell: Unable to initialise EGL".
PVRShell: EGL Error (EGL_BAD_ALLOC)
I noticed the omaplfb kernel module doesn't load:   "omaplfb: OMAPLFB_Init: OMAPLFBInit failed"
I added some kernel boot arguments for graphics memory allocation as suggested, but the module still doesn't load.
Please help. Thanks.

Here's the output of gfx_check.sh
WSEGL settings
[default]
WindowSystem=libpvrPVR2D_FRONTWSEGL.so.1
------
ARM CPU information
Processor : ARMv7 Processor rev 2 (v7l)
BogoMIPS : 718.02
Features : swp half thumb fastmult vfp edsp thumbee neon vfpv3 tls
CPU implementer : 0x41
CPU architecture: 7
CPU variant : 0x3
CPU part : 0xc08
CPU revision : 2

Hardware : am335xevm
Revision : 0000
Serial : 0000000000000000
------
SGX driver information
Version 1.6.16.4117 (release) /home/hudson/amsdk-nightly-build/cortex-A8/arago-tmp/work/am335x-evm-arago-linux-gnueabi/omap3-sgx-modules-4.05.00.03-r9e/Graphics_SDK_4_05_00_03/GFX_Linux_KM
System Version String: None
------
Framebuffer settings
open /dev/fb0: No such file or directory
------
Rotation settings
cat: can't open '/sys/class/graphics/fb0/rotate': No such file or directory
------
Kernel Module information
Module Size Used by
pvrsrvkm 145014 0
g_mass_storage 37726 0
------
Boot settings
console=ttyO0,115200n8 mem=256M vram=12M omapfb.vram=0:4M,1:3M,2:3M omapdss.def_disp=dvi root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait ip=none
------
Linux Kernel version
Linux am335x-evm 3.1.0 #1 Thu Dec 15 12:42:40 CST 2011 armv7l unknown