sir,
I am working on the above mentioned board of yours(mentioned in the subject)
i need some help regarding the porting of the linux kernel version on the board..
The board is null and void as of now..meaning...there is nothing on it at this moment..not even bootloader...
i have already compiled a bootloader(DAS U-BOOT v1.6)...
i am making use of the flash utility "OST" to load it on the board.....using USB interface...!!
I am gettin problems with drivers needed for the same...
when i plug the usb cable in the slot...my device is not recognized...i tried using the driver provided in the package of OST....but its not wroking...
plz help me out with the flash tool....!!!
regards...