Hello,
I'm using Texas Instruments 'Code Composer Studio (CCS) (figure 1), with the SDK “mcu_plus_sdk_am62px_11_01_01_08” to run examples on the AM62P.
Figure 1 - CCS Version
I'm trying to connect to the MCU_R5FSS0_0 core, but the IDE always returns the error below:
Figure 2 - Error connecting to MCU
I tried lowering the TCLK frequency, but without success as well:
Figure 3 - Connection Properties
An interesting detail is that I can connect to the WKUP_R5FSS0_0, as shown in figure 4:
Figure 4 - Connection to WKUP_R5FSS0_0
I'm running these tests on the SK-AM62P-LP evaluation board.
I tried connecting both with the built-in XDS110 and with an external one we have here, but the results were the same.
Any suggestions for additional tests I can do?