Hi i have the following queries and i am looking for any to revert , so we can plan to buy TMDXEVM8168 or TMDXEVM8148.
1. How many Digital Input, Digital Output, Analog input and Analog Output lines are there in this board?
2. How should the board be powered on? What is the rating of the power chord?
3. Will the board support the integration and working of third party libraries?
4. Is there any encoder enabled DC motor drive module that can be interfaced with this board? If so kindly suggest the same.
my application is machine -vision project using gigabit camera interface .
linux OS required . image processing algorithms will be developed by us..
pls advice on the above queries ...!