Part Number: AM62A7
Dear experts,
I am designing a system with 2 camera, 1 PCBA and 1 display. The display shall show a blending view of the two cameras.
The two camera, one is OV 0x03C10+953: MIPI RAW/60fps, another is IMX623+953: MIPIRAW/60fps.
The deserializer is 954.
What my question is the ISP function in AM62A7, as I checked data sheet for there is a VPAC module in it. I want confirm that: Is the SOC working proccess on ISP:
- tuning the first camera data at T0.
- after T0, within 1 frame time(16.67ms), camera 2 will be tunned.
Is the process right? If it is right, how can I predict the time cost on the tuning of the two cameras?
As for the two camera will be different configuration, is the VPAC will take two set of config to achieve both camera tuning?