Part Number: AM6422
Hi,
question as title, does remoteproc driver checks R5 firmware with crc, or md5, or other?
I check the source code of remoteproc driver, it has some header checks(like file size, magic ID, etc.),
but no file integrity check, right?
So, if I want to check the if the R5 firmware damaged, I have to add it by myself?
My kernel version is 6.1.90
Thanks!