Part Number: MCU-PLUS-SDK-AM64X
Other Parts Discussed in Thread: SYSCONFIG, AM6411
Hello,
My customer has a question for MCU-PLUS-SDK-AM64X.
According to the below site,
the below flash devices are supported.
- S28HS512T (1.8V)
- S25HL512T (3.0V)
Then they are asking if the below part numbers also can be supported with the same Sysconfig configuration.
- S28HL512T (3.0V)
- S25HS512T (1.8V)
Does the SDK also support these part numbers without any sysconfig modification?
They are using AM6411.
Regards,
Oba