This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VL-Q1: Regarding using TVI camera (YUV) on TDA4VL

Part Number: TDA4VL-Q1

Hi Expert,

 

Currently, the cameras used on TDA4 are Serdes Cameras, such as the IMX390 supported in the RTOS SDK and the ISX021 (YUV output) that we use.

If I want to use multi-channel TVI cameras on the Capture Node architecture of Vision apps:

1. Do you have experience using this method or customers use it?

2. We want the TVI decoder to output CSI2 YUV format directly. Are there any hardware or software reference designs we can refer to? For example, the model of the TVI decoder used, its driver in the RTOS, and its integration with the CSI driver, sensor framework, capture node, etc.

 

 

Thanks

 

Daniel