TDA4VM: Where can I download the SDK that runs the TDA4VM processor (Part No. J721EXSKG01EVM)?

Part Number: TDA4VM


www.ti.com/.../11.01.00.04
I wrote the software to an SD card and started it up, and it appears to have started up on the console, but
after a while the system reboots and doesn't work properly.

  • Hi Masao,

    www.ti.com/.../quote]

    This is the current latest SDK release and is designed to run on the J721E EVM, we will be releasing the 11.02 SDK next week.

    I wrote the software to an SD card and started it up, and it appears to have started up on the console, but
    after a while the system reboots and doesn't work properly.

    Please provide additional detail, it is not clear what firmwares or overall stack you are running. 

    The above is just the RTOS SDK, what HLOS are you using on the A72-side?

    All the J721E/TDA4VM related SDKs are listed here: PROCESSOR-SDK-J721E Software development kit (SDK) | TI.com. You would also have to use the appropriate Linux or QNX SDK depending on your HLOS choice.

    regards

    Suman

    [/quote]
  • Hi Suman.

    Thank you for your reply.

    I downloaded
    ti-processor-sdk-linux-adas-j721e-evm-11_01_00_03-Linux-x86-Install.bin — 2417019 K
    from the URL you provided and ran create-sdcard.sh in
    ti-processor-sdk-linux-adas-j721e-evm-11_01_00_03/bin$
    to write the data to the SD card.

    The console log displayed on the board is shown below.
    Is there something wrong with the way I set up my environment?

    =================
    U-Boot SPL 2025.01-00551-g743712b9ee4b (Jul 31 2025 - 11:32:44 +0000)
    SYSFW ABI: 4.0 (firmware rev 0x000b '11.1.8--v11.01.08 (Fancy Rat)')
    Trying to boot from MMC2
    Skipping authentication on GP device
    Skipping authentication on GP device
    Skipping authentication on GP device
    Skipping authentication on GP device
    Skipping authentication on GP device
    Loading Environment from nowhere... OK
    Starting ATF on ARM64 core...

    NOTICE: BL31: v2.13.0(release):v2.13.0-259-ge0c4d3903b-dirty
    NOTICE: BL31: Built : 07:01:36, Jul 1 2025
    I/TC:
    I/TC: OP-TEE version: 4.6.0-dev (gcc version 13.4.0 (GCC)) #1 Fri Apr 25 11:17:5 3 UTC 2025 aarch64
    I/TC: WARNING: This OP-TEE configuration might be insecure!
    I/TC: WARNING: Please check optee.readthedocs.io/.../ porting_guidelines.html
    I/TC: Primary CPU initializing
    I/TC: GIC redistributor base address not provided
    I/TC: Assuming default GIC group status and modifier
    I/TC: SYSFW ABI: 4.0 (firmware rev 0x000b '11.1.8--v11.01.08 (Fancy Rat)')
    I/TC: Activated SA2UL device
    I/TC: Fixing SA2UL firewall owner for GP device
    I/TC: Enabled firewalls for SA2UL TRNG device
    I/TC: SA2UL TRNG initialized
    I/TC: SA2UL Drivers initialized
    I/TC: HUK Initialized
    I/TC: Primary CPU switching to normal world boot

    U-Boot SPL 2025.01-00551-g743712b9ee4b-dirty (Jul 31 2025 - 11:32:44 +0000)
    SYSFW ABI: 4.0 (firmware rev 0x000b '11.1.8--v11.01.08 (Fancy Rat)')
    DM ABI: 3.0 (firmware ver 0x000b 'PSDK.11.01.00.04--v11.01.08a' patch_ver: 8)
    Trying to boot from MMC2
    Skipping authentication on GP device
    Skipping authentication on GP device


    U-Boot 2025.01-00551-g743712b9ee4b-dirty (Jul 31 2025 - 11:32:44 +0000)

    SoC: J721E SR1.1 GP
    Model: Texas Instruments J721e EVM
    Board: J721EX-SK rev A
    DRAM: 2 GiB (total 4 GiB)
    Core: 149 devices, 36 uclasses, devicetree: separate
    Flash: 0 Bytes
    MMC: mmc@4f80000: 0, mmc@4fb0000: 1
    Loading Environment from nowhere... OK
    In: serial@2800000
    Out: serial@2800000
    Err: serial@2800000
    am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA8 0100 ale_ver: 0x00293904 Ports:1
    Net: eth0: ethernet@46000000port@1
    Hit any key to stop autoboot: 0
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 119
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 75
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    ** Bad device specification mmc 1 **
    Couldn't find partition mmc 1:2
    Can't set block device
    libfdt fdt_check_header(): FDT_ERR_BADMAGIC
    No FDT memory address configured. Please configure
    the FDT address via "fdt addr <address>" command.
    Aborting!
    Bad Linux ARM64 Image magic!
    Scanning for bootflows in all bootdevs
    Seq Method State Uclass Part Name Filename
    --- ----------- ------ -------- ---- ------------------------ ------------ ----
    Scanning bootdev 'mmc@4fb0000.bootdev':
    __omap24_i2c_xfer_msg: error waiting for ACK (status=0x116)
    omap_i2c_xfer: errored out at msg 0: -121
    pca953x gpio@22: Error reading output register
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 76
    Scanning bootdev 'mmc@4f80000.bootdev':
    Card did not respond to voltage select! : -110
    mmc_init: -95, time 38
    Bus usb@6400000: cdns-usb3-host usb@6400000: DRD version v1 (ID: 0004024e, rev: 00000200)
    Register 2000840 NbrPorts 2
    Starting the controller
    USB XHCI 1.00
    scanning bus usb@6400000 for devices... 2 USB Device(s) found
    k3-navss-ringacc ringacc@2b800000: Ring Accelerator probed rings:286, gp-rings[9 6,20] sci-dev-id:235
    k3-navss-ringacc ringacc@2b800000: dma-ring-reset-quirk: disabled
    am65_cpsw_nuss_port ethernet@46000000port@1: K3 CPSW: rflow_id_base: 3
    ethernet@46000000port@1 Waiting for PHY auto negotiation to complete.
    ........ TIMEOUT !
    am65_cpsw_nuss_port ethernet@46000000port@1: phy_startup failed
    am65_cpsw_nuss_port ethernet@46000000port@1: am65_cpsw_start end error
    BOOTP broadcast 1
    BOOTP broadcast 2
    BOOTP broadcast 3
    BOOTP broadcast 4

    =====================-
    regards
    Masao Takayama

  • Hi Masao,

    Is there something wrong with the way I set up my environment?

    The basic steps you followed are alright.

    Do you have another board where you can try this same SDCard?

    Is this a new board that you are trying to boot, or have you used this board successfully previously?

    I recommend that you re-seat the SoM once to make sure it is not loose, pressing all 4 sides and tightening the screws a bit. 

    regards

    Suman

  • Hi Suman.
    
    Thank you for your reply. This is a new board.
    Also, we do not have the same board.
    
    >I downloaded ti-processor-sdk-linux-adas-j721e-evm-11_01_00_03-Linux-x86-Install.bin — 2417019 K from the URL you provided,
    >and ran create-sdcard.sh in ti-processor-sdk-linux-adas-j721e-evm-11_01_00_03/bin$ to write data to the SD card.
    When selecting the shell, I got a problem log when using tisdk-adas-image, but it started up successfully when using tisdk-tiny-image.
    
    This may be different, but I'm suspicious of the DT tree settings. Is that the case?
    
    regards
    Masao Takayama
  • Hi Masao,

    Just to confirm, is it that the board boots up succesfully with 

    tisdk-tiny-image but fails withe the tisdk-adas-image.

    Regards
    Gokul Praveen