This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: Confirmation of TDA4VH Encoding Capability for Multi-Channel Use Case

Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH

1.jpg

2.jpg

We are currently developing a system based on TDA4VH and would like to confirm its video encoding capability.
Based on the documentation, TDA4VH integrates two video encoder cores. For an encode-only use case, is it correct to understand that:

  • The total equivalent encoding throughput is 2 × 4K@60, and
  • The total number of encoding instances is ≤ 64 ?

Under the above assumptions, we would like to confirm whether TDA4VH can support the following encoding workload:

  • Codec: H.265 / HEVC

  • Profile: HEVC_MAIN

  • Level: 5.1

  • Rate Control Mode: LOW_LATENCY

Encoding channels (all at 20 fps):

  • 13 × 1280×720

  • 1 × 1024×576

  • 2 × 576×648

  • 2 × 480×288

  • 4 × 960×768

  • 1 × 640×512

  • 1 × 512×896

The total encoding load is estimated to be approximately 35% of the 2 × 4K@60 equivalent throughput, with 24 encoding instances in total.

Could you please confirm whether this workload is supported, and whether there are any additional limitations (e.g., per-core channel limits, driver/firmware constraints, or CMA memory requirements) that we should be aware of?

Thank you.