Hi,
when i am running ./moduletest.out drv_isifi i m getting the following output.
# ./moduletest.out drv_isif
CLK Hz,
ARM Hz = 432000000
DDR Hz = 340000000
VPSS Hz = 340000000
IMCOP Hz = 340000000
DRV LDC: GetConfig 0003 0x0
[OSA_FILE ] Reading file [/mnt/nand/IMG_Paramset.bin] ... Done. [1683076 bytes]
ISIF: Opening imager.
############OPEN###########
==========>>>> Start X,Y = 52,18
Sensor Mode Info,
Width = 744
Height = 516
fps = 30
Bin Enable = 0
Sensor Frame Timing Info,
fps = 30
t_frame (ns) = 33333334.000000
t_row (ns) = 25687.500000
t_pclk (ns) = 15.625000
W = 744
H = 516
SW = 1125
SD = 0
HB = 450
VB = 781
HBmin = 450
VBmin = 9
f_pclk = 64000000
shutterOverhead (ns) = 6656.250000
col_size = 744
row_size = 516
col_bin = 0
row_bin = 0
col_start = 728
row_start = 652
pll_M = 16
pll_N = 1
pll_DIV = 1
############reset###########
############SPI OPEN###########
spi mode: 16
bits per word: 8
max speed: 12000000 Hz (12000 KHz)
############SET REG###########
############OPEN END###########
ISIF: Opening ISIF.
================> 512, 0, 1735
ERROR (drv_isif.c|DRV_isifSetParams|679): CSL_ccdcBufInit()
ERROR (drv_isif.c|DRV_isifOpen|131): DRV_isifSetParams()
ISIF: Closing imager.
ISIF: Exiting.
Any reasons for this error.
Thanks