This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI problem during video encoding(h264)

Hello Community,

I am working on a h264 video encoding project on the DM6467 platform. Based on the demo applications from the dvsdk, i started developing a user space application for video encoding. The last weeks i worked on a linux kernel module which implements a spi protocol driver. My userspace application handles the video data trough a ioctl to my kernelmodul, which transfers the data trough spi towards a FPGA.

The kernelmodul stores video data in kernelspace (CopyFromUser) and the ioctl returns to userspace immediatly. The kernelmodule registers an interrupt on a GPIO. After it is receiving a interrupt from the FPGA, it starts transfering the a video data block of 1024 bytes to the FPGA. While driving this module from an test application, my spi protocol driver works fine. When i start using my video encoding application i get following kernel messages:

"spi_davinci spi_davinci.0: SPI data transfer error"

With a IRQ frequency smaller than 700 Hz i get the above message. The occurrenceof this message unpredictabled, but it appears several times per second. My video bitrate is about 4Mbit. And again: the message does not occur if i use my test application. So i guess its a problem with only occurs during video encoding.

I read  trough the davinci_spi.c code, i found that the above message is printed if the DMA transfer fails. Is it possible, that a video codec disturbs my spi dma transfers? Has anybody some advices for me?

Thanks!