Other Parts Discussed in Thread: TVP5158
Hi ,
I have a custom board which consists of TI8148 and TVP5158.
I tried to use the DM365_DVR_DVSDK3_00.02.00.00 package for patching the kernel .
when i try to compile the kernel (uImage) with or without TVP5158 support i get an error .
the questions are :
1. how can i change the patch to work with sdk 4 ? or kernel 2.6.37 ?
2. there is any stand alone driver ? because the DM365_DVR_DVSDK3_00.02.00.00 consists a lot of files ..
- for any idea's please send me mail to avisdb@gmail.com .
thank you .