This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power voltages for VDD_CORE and VDD_MPU

I would like to use the AM335x at maximum frequency (720MHz) and in deep sleep mode.

Do I have to set the VDD_CORE to 0.95V, or can I leave it at 1.1V always? If I don't care about a little higher power consumption? Will it work in deep sleep mode at VDD_CORE = 1.1V?

The VDD_MPU voltage I should change between 0.95V and 1.26V. Am I right?

I want to decrease the number of different power voltages.