This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: AM625: I2C driver crash at boot time with tisdk11 linux

Part Number: AM625

Hello Nick,

Here is my answer regarding the previous thread 1586971.

Do you also see the behavior with SD card boot instead of NFS?

The issue doesn't not occurs when using SD Card or internal flash.

But our flashing process requires that Linux OS run from NFS to be able to flash the internal flash, the OTP and the eeprom.

Could you tell us what can be done to bypass the issue ?

Regards,

Nick