This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Storing Data from DMA to SD Card

Hi All,

I've been working with the CSL and managed to make a project that saves ASCII characters to the SD Card through the CSL & BIOS. I have also worked on another project (which is basically a cut down version of the Audio Filter demo) to retrieve data from the Codec using DMA. I wish to combine these two projects, so that i may save this data to the SD card continuously. However whenever I try to bring the attached code into a project with BIOS/CSL it no longer works. Could someone please point me in the right direction of adapting the code to work with CSL & BIOS, ultimately I'm basically trying to sample from the Codec using I2S/DMA and save the data to the SD Card.

Attached is the project for the I2S/DMA project.7418.DMAPingPOng.zip

Kind Regards

James