Part Number: TMDSEVM572X
Other Parts Discussed in Thread: AM1802
This post uses a translation.
Hello
I'm trying to debug the TMDSEVM572x SBL using the XDS200 emulator. I installed CCS on Ubuntu and ran Test Connections, but the connection doesn't terminate correctly.
I followed the steps below, referring to a lot of information on the forum.
I couldn't find anything similar to the problem I'm currently experiencing, so I posted here.
Is there something I've overlooked or anything else I need to do? Any advice would be appreciated.
I was wondering whether I should contact Blackhawk support, so I posted here.
https: //www.blackhawk-dsp.com/support
■EVM
TMDSEVM572x
■Emulator
XDS200 DEBUG PROBE (TMDSEMU200-J)
■Host PC: Windows11 VirtualBox
Version: 7.1.10 r169112 (Qt6.5.3)
■Host OS: Ubuntu18.04
xds2xx@xds2xx-VirtualBox: ~$ hostnamectl
Static hostname: xds2xx-VirtualBox
Icon name: computer-vm
Chassis: vm
Machine ID: fc8cc8ae154240f1b1b255c557bb13e8
Boot ID: 9742725a501e4613837c9f8c9d83938d
Virtualization: oracle
Operating System: Ubuntu 18.04.6 LTS
Kernel: Linux 5.4.0-150-generic
Architecture: x86-64
xds2xx@xds2xx-VirtualBox: ~$
■Procedure
Step1: Install CCS12.8.1 on Ubuntu18.04
Step2: Checking ModemManager Status
sudo systemctl status ModemManager.service
Loaded: loaded (/lib/systemd/system/ModemManager.service; enabled; vendor preset: enabled)
Active: active (running) since .....
CGroup: /system.slice/ModemManager.service --889 /usr/sbin/ModemManager --filter-policy=strict
Step3: Change ModemManager policy
sudo nano /lib/systemd/system/ModemManager.service
ExecStart=/usr/sbin/ModemManager --filter-policy=default
Step4: Reload the systemd service, restart ModemManager. I also rebooted my system just in case.
sudo systemctl daemon-reload
sudo systemctl restart ModemManager
Step5: Run ./install_drivers.sh
go to <CCS_INSTALL_DIR>/ccs/install_scripts
sudo ./install_drivers.sh
Step6: Add a user to the dialout group
sudo usermod -aG dialout $USER
Step7: Connect the xds200 emulator to the EVM, connect the USB of the xds200 emulator to the PC, and turn on the EVM.
J5 on the EVM is connected
From the VirtualBox menu, select <Device> -> <USB> -> <Spectrum Digital XDS2xx USB Emulator – Composit [0100]>
Step8: Test the debug probe
cd ti/ccs1281/ccs/ccs_base/common/uscif/xds2xx/
./xds2xx_conf get xds2xxu 0
xds2xx@xds2xx-VirtualBox: ~/ti/ccs1281/ccs/ccs_base/common/uscif/xds2xx$ ./xds2xx_conf get xds2xxu 0
boardRev=2
ipAddress=0.0.0.0
ipConfig=dhcp
ipGateway=255.255.255.255
ipNetmask=255.255.255.255
productClass=XDS2XX
productName=XDS200
serialNum=S200-000FD2066413
swRev=1.0.0.9
hostCPU=AM1802
emuCtrlType=Bit bang
extMemType=SDRAM
portUSB=true
portENET=false
portWIFI=false
portRS232=false
EnableUSBSerial=true
CurrentMeasure=false
xds2xx@xds2xx-VirtualBox: ~/ti/ccs1281/ccs/ccs_base/common/uscif/xds2xx$
*However, the above command works fine only once. If you run it a second time, it will freeze. Therefore, you will need to attach the USB device again in step 7.
Step9: Run CCS1281 and follow the steps below:
Step9-1: <View> -> <Target Configurations> -> <Projects> -> <New Target Configuration> -> Create Test.ccxml
Step9-2: In Basic General Setup
Connection: Texas Instruments XDS2xx USB Debug Probe
Board or Device: DRA72x
Save Configuration -> Save
Step9-3: Select <Test Connection> -> <Test Connection> or
<Advanced Setup> -> <Target Configuration> -> <All Connections> -> <Texas Instruments XDS2xx USB Debug Probe_0>
< Execution result>
[Start: Texas Instruments XDS2xx USB Debug Probe_0]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
/home/xds2xx/.ti/ccs1281/0/0/BrdDat/testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
The library build date was 'Sep 26 2024'.
The library build time was '14: 57: 19'.
The library package version is '20.0.0.3178'.
The library component version is '35.35.0.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '13' (0x0000000d).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
This emulator does not create a reset log-file.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open: : dtc_io
Failed to open i/o connection (xds2xxu: 0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the debug probe via USCIF ECOM has failed.
[End: Texas Instruments XDS2xx USB Debug Probe_0]
========
It works fine on Windows 11 and CCS 12.7.1.
(Even if it crashes on Ubuntu, xds2xx_conf get xds2xxu 0 works fine on Windows 11.)
Step 8, Test the debug probe, can also be run multiple times.