Hello,
I am trying to boot my DM365 EVM board over the network for the first time, and the following error appears:
-----------------------
RAMDISK: Couldn't find valid RAM disk image starting at 0.
Root-NFS: No NFS server available, giving up.
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "/mtdblock4" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
1f00 15360 mtdblock0 (driver?)
1f01 1024 mtdblock1 (driver?)
1f02 4096 mtdblock2 (driver?)
1f03 524288 mtdblock3 (driver?)
1f04 1552384 mtdblock4 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
-----------------------
For reference, I've pasted my environment variables here:
-----------------------
ethaddr=00:0e:99:02:c9:19
bootdelay=4
baudrate=115200
bootfile=uImage-dm365-evm.bin
serverip=192.168.1.142
bootcmd=dhcp;tftpboot;bootm
bootargs=mem=116M console=ttyS0,115200n8 root=/mtdblock4 rw initrd=0x82000000,4M ip=off
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 1.3.4 (May 22 2009 - 11:25:39)
Environment size: 306/262140 bytes
-----------------------
Prior to booting, I ran the ./setup.sh script in ./dvsdk/ and chose the defaults for all of the settings. Is there another step I need to take?
Any help is appreciated, thank you.