Part Number: AM67A
Other Parts Discussed in Thread: J722SXH01EVM,
Development Board: J722SXH01EVM
"uname -r" : 6.12.17-ti-00773-gcdcaeac783e3-dirty
image: tisdk-edgeai-image-j722s-evm.wic.xz
Hello,
I am working with the J722SXH01EVM evaluation board. This board uses the same processor as a custom embedded board currently under development, and I am testing and comparing certain properties between the two platforms.
I am using the following SD card image on the EVM:
-
tisdk-edgeai-image-j722s-evm.wic.xz(~1.04 GB),
from Processor SDK Linux for AM67A → SD card image with Edge AI stack
To test additional external/attachment modules on the board, I need to build some out-of-tree kernel modules (.ko).
I attempted to compile the module sources directly on the development board, but the Linux kernel headers are not present in the filesystem.
My questions are:
-
What is the recommended way to obtain the correct Linux kernel headers or kernel source for this image in order to compile kernel modules?
-
Is it mandatory to use the Yocto SDK for building kernel modules?
-
Is there an alternative method to compile kernel modules without installing the full Yocto SDK, as its size is quite large?
Any guidance or best-practice recommendations would be appreciated.
Thank you.
Best regards,
Hasan Halil