Part Number: AM62A7
We are trying to bring up an optical path with the following configuration
- Deserializer: Maxim 9296
- Serializer : Maxim 9295x2 ( 2 camera)
As part of the bringup we haven't implemented Linux driver for those serdes yet but using shell script for initialization instead
We have driver ready for the sensors though, and we have confirmed both works.
Our questions are:
- What do we need to change in device tree/boot overlay to make the 2 cameras available in media topology
- What changes needed in CSI2RX to accept CSI 2 with 2 streams
- Have you implemented kernel driver for this serdes pair? and will this be available anytime soon
- Any sample code we could use as reference
Thank you