This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517: De-interlace function

Guru 10255 points

Other Parts Discussed in Thread: AM3517

Hi.
I would like to make sure De-interlace function in AM3517 TRM;
10.3.2.1.4.4 Line Output Control, page-1143.
http://www.tij.co.jp/jp/lit/ug/sprugr0b/sprugr0b.pdf

The interlacing is that just takes the odd and even fields
but it is not consider that combines them into a single frame with
some processing that will smooth out the offsets between the two fields
(which is most pronounced when there is lot of motion). 

Is my understanding correct?

If so, when I would like to remove some saw tooth (combing) noises from images,
do I need the other device to de-interlace with functions to interpolate the missing lines
from the original field?

Regards,
Kanae