Is it possible to create an RTSC/SYS/BIOS project for the C5535 device?
When I create the project, if I set the device to TMS320C5535 the RTSC target is empty, and that later creates problems. If I choose TMS320C5505 instead, the target defaults to ti.targets.C55_large, which later indicates "Target not supported ti.targets.C55_large".
I notice that the C5535 USB devkit comes with a DSP/BIOS 5 project, not a SYS/BIOS project...
Thanks for the help Bruno