Part Number: AUDIO-AM62D-EVM
Hello team,
What I did:
- Execute installer (ti-processor-sdk-linux-am62dxx-evm-11.02.08.02-Linux-x86-Install.bin) in arbitrary directory inside Ubuntu Linux VM. Note I have chosen not to download Docker image. This would raise potentially problems in intranet.
- I skipped NFS, TFTP and u-boot configuration steps. My idea is to build first images suitable for putting on SD card. Maybe later the other options could be considered.
- Then I proceeded as mentioned in SDK documentation (1.1.4 SDK Build using Makefile).
I stepped into top level and executed: “make clean” and “make all” – build everything. - This starts but stops after building several artifacts
/data2/wksp-am62d-01/sdk-am62d-2/board-support/ti-u-boot-2025.01+git/tools/mkeficapsule.c:20:10: fatal error: gnutls/gnutls.h: No such file or directory
20 | #include <gnutls/gnutls.h>
| ^~~~~~~~~~~~~~~~~
compilation terminated.
make[3]: *** [scripts/Makefile.host:112: tools/mkeficapsule.o] Error 1
make[3]: *** Waiting for unfinished jobs....
make[2]: *** [/data2/wksp-am62d-01/sdk-am62d-2/board-support/ti-u-boot-2025.01+git/Makefile:1918: tools] Error 2
make[2]: Leaving directory '/data2/wksp-am62d-01/sdk-am62d-2/board-support/u-boot-build/r5'
make[1]: *** [Makefile:177: sub-make] Error 2
make[1]: Leaving directory '/data2/wksp-am62d-01/sdk-am62d-2/board-support/ti-u-boot-2025.01+git'
make: *** [makerules/Makefile_u-boot:41: u-boot-r5] Error 2
Perhaps this is not the right way to proceed.
At the end I want to be able to
- Add additional packages to “default” target (tools, libs, other)
- Adapt drivers for McASP to prepare for “our” data format
- Maybe need to adapt u-boot parameters
- Maybe need to rebuild Linux kernel
- I don’t want to (re)build R5
Perhaps I should start better with “1.2. Building the SDK with Yocto”?
Best regards,
Til