I'm coming back around to try and diagnose why only 20% of my identical prototype boards work. The problem is that I can't even connect to the target using CCSv4, using the JTAG connection. My few working boards do this successfully, but all the others fail.
I believe the problem is that my fab line is having trouble with the BGA assembly. But even with a random number of failures (more likely open circuits than short circuits), I would think I would have a higher number of boards to which I could at least connect. After all, only a FEW pins are needed for this.
With the above in mind, I'm trying to figure out what are the MINIMUM aspects of the TMS320DM6467ZUT7 board that need to be working. Please consider the following, and tell me if there's something else that needs to be working.
- Both 1.2XV and 3.3V power supplies. (WHICH of the multiple power and ground pins simply MUST be successfully connected?)
- 27MHz primary crystal circuit (two pins). This is to the EXCLUSION of the aux crystal circuit. (Or does JTAG work with no crystal operating at all?)
- JTAG connections
I can't imagine that anything else is required. (I would enumerate the pins above in more detail, but my schematic program is crashed at the moment, so I can't consult my schematic. Conceptually, isn't power, crystal, and JTAG all the connections required? This should be only 7 pins or so, plus power and ground.
Please suggest exact which minimum set of pins must be successfully connected in order to connect to the target using CCSv4.
Thanks very much,
Helmut