Part Number: AM2754-Q1
Hi,
I am using the C7x core of the AM2754. When the .cio section is placed in L2SRAM, there is no issue, but when it is placed in MSRAM, the following problem occurs:
Invalid CIO command (2) in the CIO buffer at address (0x80200000) was not recognized. Please disable interrupts while running.
Both L2RAM and MSRAM are configured as Outer Shareable, Normal outer and inner write-back cacheable non-transient memory.
Is the .cio section required to be placed only in L2SRAM?