This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J784S4XEVM: Kernal Initialization Failed

Part Number: J784S4XEVM

I already compiled model artifacts under tidl_artifacts. When I run this  code on the PC Emulation mode it works. When I run this under on the EVM board I get kernal initialization errors during sess.run. Can I please have some guidance? image.png

provider_options = {
    "tidl_tools_path": os.environ["TIDL_TOOLS_PATH"],
    "artifacts_folder": "tidl_artifacts",
    "tensor_bits": 32,
    "advanced_options:inference_mode": 0,
    "advanced_options:num_cores": 4,
}

sess = rt.InferenceSession(
    model_path,
    providers=["TIDLExecutionProvider", "CPUExecutionProvider"],
    provider_options=[provider_options, {}],
)

print("Providers provided:", sess.get_providers())

# inference test
w = np.zeros((1, 4), dtype=np.float32)
x = np.array([2.5], dtype=np.float32)
y = np.random.randn(1, 64).astype(np.float32)
z = np.zeros((1, 2, 64), dtype=np.float32)


outputs = sess.run(
    None,
    {
        "w": w,
        "x": x,
        "y": y,
        "z": z,
    }
)

print("new_state:", outputs[0])
print("rnn_next_state shape:", outputs[1].shape)