Other Parts Discussed in Thread: TVP5146, TVP7002, THS7353
hi
i m trying to develop support for mt9v113 sensor in my leopard board dm365
for that i found mt9v113.c and related heder files on net
i hve updated kconfig and makefile to inset the support as module
this the changes i ve done in my board-dm365-leopard.c
#if defined(CONFIG_VIDEO_MT9V113) || defined(CONFIG_VIDEO_MT9V113_MODULE) //by me
static struct v4l2_input mt9v113_inputs[] = {
{
.index = 0,
.name = "Camera",
.type = V4L2_INPUT_TYPE_CAMERA,
}
};
#endif
static struct vpfe_subdev_info vpfe_sub_devs[] = {
#if defined(CONFIG_VIDEO_TVP514X) || defined(CONFIG_VIDEO_TVP514X_MODULE)
{
.module_name = "tvp5146",
.grp_id = VPFE_SUBDEV_TVP5146,
.num_inputs = ARRAY_SIZE(tvp5146_inputs),
.inputs = tvp5146_inputs,
.routes = tvp5146_routes,
.can_route = 1,
.ccdc_if_params = {
.if_type = VPFE_BT656,
.hdpol = VPFE_PINPOL_POSITIVE,
.vdpol = VPFE_PINPOL_POSITIVE,
},
.board_info = {
I2C_BOARD_INFO("tvp5146", 0x5d),
.platform_data = &tvp5146_pdata,
},
},
#endif
#if defined(CONFIG_VIDEO_TVP7002) || defined(CONFIG_VIDEO_TVP7002_MODULE)
{
.module_name = "tvp7002",
.grp_id = VPFE_SUBDEV_TVP7002,
.num_inputs = ARRAY_SIZE(tvp7002_inputs),
.inputs = tvp7002_inputs,
.ccdc_if_params = {
.if_type = VPFE_BT1120,
.hdpol = VPFE_PINPOL_POSITIVE,
.vdpol = VPFE_PINPOL_POSITIVE,
},
.board_info = {
I2C_BOARD_INFO("tvp7002", 0x5c),
.platform_data = &tvp7002_pdata,
},
},
{
.module_name = "ths7353",
.grp_id = VPFE_SUBDEV_TVP7002,
.board_info = {
I2C_BOARD_INFO("ths7353", 0x2e),
},
},
#endif
#if defined(CONFIG_SOC_CAMERA_MT9P031) || defined(CONFIG_SOC_CAMERA_MT9P031_MODULE)
{
.module_name = "mt9p031",
.is_camera = 1,
.grp_id = VPFE_SUBDEV_MT9P031,
.num_inputs = ARRAY_SIZE(mt9p031_inputs),
.inputs = mt9p031_inputs,
.ccdc_if_params = {
.if_type = VPFE_RAW_BAYER,
.hdpol = VPFE_PINPOL_POSITIVE,
.vdpol = VPFE_PINPOL_POSITIVE,
},
.board_info = {
I2C_BOARD_INFO("mt9p031", 0x48),
// this is for PCLK rising edge //
.platform_data = (void *)1,
},
},
#endif
#if defined(CONFIG_VIDEO_MT9V113) || defined(CONFIG_VIDEO_MT9V113_MODULE) //by me
{
.module_name = "mt9v113",
.is_camera = 1,
.grp_id = VPFE_SUBDEV_MT9V113,
.num_inputs = ARRAY_SIZE(mt9v113_inputs),
.inputs = mt9v113_inputs,
.ccdc_if_params = {
.if_type = VPFE_YCBCR_SYNC_8,
.hdpol = VPFE_PINPOL_POSITIVE,
.vdpol = VPFE_PINPOL_POSITIVE,
},
.board_info = {
I2C_BOARD_INFO("mt9v113", 0x3c),
// this is for PCLK rising edge /
.platform_data = (void *)1,
},
}
#endif
};
but its not detecting anything while boot up
the boot up message for vpfe _capture is
vpfe_init
vpfe-capture: vpss clock vpss_master enabled
vpfe-capture vpfe-capture: v4l2 device registered
vpfe-capture vpfe-capture: video device registered
No sub devices registered
vpfe-capture: vpfe capture clocks disabled
vpfe_register_ccdc_device: DM365 ISIF
dm365_isif: probe of dm365_isif failed with error -22
af major#: 252, minor# 0
AF Driver initialized
aew major#: 251, minor# 0
AEW Driver initialized
its not detecting the censor that i ve attached to the board
thanxx
kailash