We are facing issue when we press the POWER button to resume from suspend mode, when the system is in low power
Kenrel:3.0.8; omap4460: ES1.1; android: 4.0.1
Seeing this message in console...
---------------------------------------------------------
...
Resume caused by IRQ 69, gp timer
.
.
Powerdomain (core_pwrdm) didn't enter target state 1 Vs achived state 3. current state 3
Powerdomain (mpu_pwrdm) didn't enter target state 1 Vs achived state 3. current state 3
Powerdomain (l4per_pwrdm) didn't enter target state 1 Vs achived state 3. current state 3
Could not enter target state in pm_suspen.
----------------------------------------
from the log it looks to me that, it did not goto the supend state at all. but while pressing the power button it does not wake-up
Could you please get back if someone faced this similar issue? In case need further debug info i can post it over here...
Thanks
Venkat