Part Number: AM623
Hi Team,
We have a requirement to access the LAN9694 (external SoC) UART CLI from the AM623 USB interface. Due to hardware limitations, it is not possible to add a USB‑to‑UART bridge IC (such as the FT230x).
Therefore, we need to access the LAN9694 UART debug console from the AM623 USB port without adding any additional hardware ICs, using a software‑based solution instead.
Could you please share your inputs on how this requirement can be achieved?
Below Development environment using to test AM623 USB CLI
Evaluation Board:- AM62B-P1
SDK:- PROCESSOR-SDK-LINUX-RT-AM62X — Processor SDK RT-Linux for AM62x Version: 11.01.05.03
Build Environment:- Yocto build environment
Thanks & Regards,
Janani