This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The PWM outputs on AM37x/35x based on Linux



Hi, all

 

   More than several customers want to use the general purpose timers to implement the PWM outputs on AM37x/35x Linux platform.

 

   And we find that there is a simple guide on internet: http://www.jumpnowtek.com/index.php?option=com_content&view=article&id=56&Itemid=63.

 

   According to the guide, one customer, Jabil, have some try as following:

 

   /*! \fn static void lcd_set_bk_duty(int duty)

    \brief set the PWM duty of LCD backlight

    \param duty the duty to set, 0 ~ 100

*/

static void lcd_set_bk_duty(int duty)

{

    int match_value = 0;

 

    if (NULL == lcd_bk_timer)

    {

        return;

    }

 

    duty = (duty < 0 ? : (duty > 100 ? 100 : duty));

    match_value = LCD_BK_FREQ_DEF + (0xFFFFFFFE - LCD_BK_FREQ_DEF) * (100 - duty) / 100;

    omap_dm_timer_set_match(lcd_bk_timer, 1, match_value);

    omap_dm_timer_set_pwm(lcd_bk_timer, 1,  1, 1);

    omap_dm_timer_set_config(lcd_bk_timer, 0x1842);

    omap_dm_timer_start(lcd_bk_timer);

    duty_bak = duty;

}

 

  But they found that the PWM duty can’t reach 0% or 100% even through it is much closed. 

  So is there some advice for this?

  Thanks & BR !

  Yaoming