Part Number: SK-AM62B-P1
Hello,
I'm trying to setup CCS to debug my application running on M4F core of AM62X board. I installed CCS-20.4.1 and trying to run the hello_world example for M4F with FreeRTOS. I'm able to build the project but when I start the Debug session, I get this error "Unknown module: file". Any idea what this is pointing to? I went to the CCS installation folder and found that log coming from the file "ccs_base/cloudagent/src/module.js". Should I be running the cloudagent? I believe I installed everything by default and didn't see install options about cloudagent.
When I looked at the code logging that error, the comment there says to create the submodule if it hasn't been created but I don't see the code doing that:
// This sub module has not been created yet
const moduleID = moduleUniqueID++;
log(`Creating new module (module id: ${moduleID})`);
if (!(subModuleName in moduleObj.subModules)) {
throw new Error("Unknown module: " + subModuleName);
}
Am I missing something in my config? I'm attaching the launch.json file and the ccxml file I'm using (extension renamed to allow upload). Thanks in advance.
-Ayman