This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: LWIP example not working on SK-TDA4VM

Part Number: TDA4VM

Hi 

I am trying to run LWIP enet example for FreeRTOS on SK-TDA4VM. It is not able to get any IP address from DHCP. Moreover, the LEDs on Ethernet port was not blinking at all. 
I am running it on MCU2_1 using CCS work flow. 

Below is the output:
==========================
      Enet lwIP App       
==========================
EnetBoard_setupPorts: 1 of 1 ports configurations found
CPU Load: 100%
Starting lwIP, local interface IP is dhcp-enabled
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 1 To 0 
EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:1 From 1 To 0 
EnetMcm: CPSW_2G on MCU NAVSS
Mdio_open: MDIO manual mode enabled
PHY 0 is alive
EnetPhy_bindDriver: PHY 0: OUI:080028 Model:23 Ver:01 <-> 'dp83867' : OK
Host MAC address: 34:08:e1:59:db:e4
[LWIPIF_LWIP] Enet LLD netif initialized successfully
status_callback==UP, local interface IP is 0.0.0.0
CPU Load: 6%
CPU Load: 2%
CPU Load: 2%
CPU Load: 2%
CPU Load: 2%

  • Hi,

    The PSDK RTOS support for the SK-TDA4VM board is not available. It has only a Linux package.

    If you would like to use PSDK RTOS for SK-TDA4VM, you need to make board-specific changes to the examples, as this SDK is developed for the Common Processor Board (https://www.ti.com/tool/J721EXCPXEVM) +  SOM (https://www.ti.com/tool/J721EXSOMXEVM).

    Best Regards,
    Sudheer

  •   , 
    Would you please highlight the expected changes, I need to make it to work? 
    Like, pin configurations, clock configurations or anything else I need to make. 


    I was compiling the FW using the j721e_evm as board for core mcu2_1. 

    Thanks,
    Muhammad Usman

  • Hi,

    PHY is detected by MDIO, I believe clock is supplied.

    Can you please check whether  "Cpsw_periodicTick" API is called or not?  I could not see Link up here eventhough PHY is detected.

    Best Regards,
    Sudheer

  • Hi  ,

    Yes the Cpsw_periodicTick is calling properly. 

    The link status variable (linkStatus) is always  "ENETPHY_LINK_DOWN". 

    Thanks,
    Muhammad Usman

  • Hi,

    The link status variable (linkStatus) is always  "ENETPHY_LINK_DOWN". 

    It means PHY is not Link Up. Can you please read the PHY BMSR register and check whether the link is up or not? 

    Also, can you please confirm that CPSW is disabled from HLOS (Linux)?  
    Also, ensure PHY is Link Up.


    Best Regards,
    Sudheer

  •  Hi  , 


    The BMSR shows that link is down. 
    I am not running HLOS. Just FreeRTOS on MCU2_1 using CCS workflow (launch.js runs first, then reset the CPU core and then LWIP example app on MCU2_1). 

    PHY always remains in ENETPHY_FSM_STATE_NWAY_WAIT state, until the timeouts and state machine restarted. 
    I increased the timeout but same behavior. 

    Thanks,

    Muhammad Usman

  • HI, 

    The BMSR shows that link is down

    It means PHY side no Link Up with link partner.

    I am not running HLOS. Just FreeRTOS on MCU2_1 using CCS workflow (launch.js runs first, then reset the CPU core and then LWIP example app on MCU2_1)

    Understood, just running using CCS. 

    PHY always remains in ENETPHY_FSM_STATE_NWAY_WAIT state, until the timeouts and state machine restarted. 
    I increased the timeout but same behavior

    It would be due to no link-up from phy side. 

    Have you verified data transfer from CPSW 2G when loading Linux? 

    Best Regards 

    Sudheer

  • Hi,

    Yes I can see proper link up messages on Linux and DHCP works on Linux. 

    Thanks,

    Muhammad Usman

  • Hi,

    Yes I can see proper link up messages on Linux and DHCP works on Linux. 

    Understood.

    I have verified the Linux device tree for SK-EVM. I could not see any additional GPIOs used for PHY control.

    Can you please confirm whether Pinmux is configured for MCU CPSW2G as RGMII?
    Also, please share the list of changes applied to the ENET LWIP example.

    Best Regards,
    Sudheer

  • Hi,

    I added some log starting with "TRACE:". Only four lines below which shows that PINMUX is fine. 

    ==========================
    Enet lwIP App
    ==========================
    TRACE: Configuring MCU CPSW2G MAC mode=2 (RGMII=2)
    TRACE: MCU_ENET_CTRL register written with value=0x12
    EnetBoard_setupPorts: 1 of 1 ports configurations found
    TRACE: Configuring MCU RGMII pinmux (moduleId=5)
    TRACE: MCU RGMII pinmux configuration completed
    CPU Load: 39%
    Starting lwIP, local interface IP is dhcp-enabled
    EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:0 From 1 To 0
    EnetAppUtils_reduceCoreMacAllocation: Reduced Mac Address Allocation for CoreId:1 From 1 To 0
    EnetMcm: CPSW_2G on MCU NAVSS
    Mdio_open: MDIO manual mode enabled
    PHY 0 is alive
    EnetPhy_bindDriver: PHY 0: OUI:080028 Model:23 Ver:01 <-> 'dp83867' : OK
    Host MAC address: 34:08:e1:59:db:e4
    [LWIPIF_LWIP] Enet LLD netif initialized successfully
    status_callback==UP, local interface IP is 0.0.0.0
    CPU Load: 6%
    CPU Load: 2%
    CPU Load: 2%
    CPU Load: 2%

    The only change I did in file (.../enet_lwip_example/test_config_j721e.c) is: 
    #define APP_ENABLE_STATIC_CFG                      (0U)    ---->     #define APP_ENABLE_STATIC_CFG                      (1U)

    Thanks,

    Muhammad Usman

  • Hi,

    TRACE: Configuring MCU CPSW2G MAC mode=2 (RGMII=2)
    TRACE: MCU_ENET_CTRL register written with value=0x12
    EnetBoard_setupPorts: 1 of 1 ports configurations found
    TRACE: Configuring MCU RGMII pinmux (moduleId=5)
    TRACE: MCU RGMII pinmux configuration completed
    CPU Load: 39%

    If so, Pins are mapped to RGMII.

    You supposed to get PHY Link Up if its connected with Link partner.

    Best Regards,
    Sudheer

  • Hi,

    Unfortunately the link is not establishing. As soon the code runs the LEDs on RJ45 connector turn OFF, before running the example they are ON. 


    Best regards,

    Muhammad Usman

  • Hi,

    Unfortunately the link is not establishing. As soon the code runs the LEDs on RJ45 connector turn OFF, before running the example they are ON. 

    Can you please check if PHY is bootstrapped? If so, you can ignore the PHY configuration in the CPSW MAC Port configuration and use phyaddr ENETPHY_INVALID_PHYADDR, as captured below.



    Best Regards,
    Sudheer

  • Hi, 

    Setting ENETPHY_INVALID_PHYADDR didn't work. 


    Moreover, I did some debugging and observed that the Ethernet LEDs turn OFF as soon as the following function executes even I do not run the LWIP example:

    void SciApp_consoleInit(void)
    {
        Board_initCfg   boardCfg;
    
        boardCfg = BOARD_INIT_PINMUX_CONFIG |
                   BOARD_INIT_UART_STDIO;
        Board_init(boardCfg);
    }

    Simply load the launch.js file and run that code using CCS instead of resetting the core1_0.
    If I remove the BOARD_INIT_PINMUX_CONFIG from above code it keeps LEDs in ON state. 

    So I am suspecting that there is some problem in PIN configurations. I'll investigate it further in LWIP example and get back to you on it. 

    Thanks,

    Muhammad Usman

  • Hi,

    Simply load the launch.js file and run that code using CCS instead of resetting the core1_0.
    If I remove the BOARD_INIT_PINMUX_CONFIG from above code it keeps LEDs in ON state. 

    As I have mentioned earlier, RTOS SDK is not compatible for SK-EVM so, there is a expected change in Board configuration as SDK is compatible to Common processor Board.

    Please remove pin configurations from boards configurations apart from MCU CPSW2G pins.


    Best Regards,
    Sudheer