Hi,Marc
I encounter the nand read speed issue during my development, the detail
procedure as below:
1.I used the Micron Large page x16 NAND for development.
2.In \u-boot-2010.06-psp04.00.00.10\arch\arm\include\asm\arch-ti81xx\Mem.h
file , I modified the M_NAND_GPMC_CONFIG5 bit 0-4(which means RDCYCLETIME).
from 1e(default) to 07(fast speed as calculated) .
3.I print the value of M_NAND_GPMC_CONFIG5 ,lt's vaule changed as i
modified.
4. I through Oscilloscope I observed between both setting(1e and 07)
TOE(which means read cycle time) are around 632 ns.looks like the change
doesn't take the effect for the hardware.
whether any other setting i need to do to solve this issue?