Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64EVM: Query regarding the linux kernel source code provided in the Processor SDK Linux of AM64x

Part Number: TMDS64EVM

Hi Team,

 

I am working with the AM64x EVM and Processor SDK Linux(Version: 11.02.08.02).

I understand that the AM64x boot flow (SD/eMMC) uses a prebuilt kernel Image and DTB loaded by U-Boot, and that the Linux kernel source is provided for rebuild/customization as part of the SDK.

I would like to clarify the following points:

• Where exactly is the Linux kernel source code directory located inside the Processor SDK Linux installation for AM64x?

• What is the recommended way to rebuild the kernel so that the generated Image and DTBs remain compatible with the default AM64x EVM boot flow?

Regards,

Sumi