This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AEN-Q1: [J722S] kernel log have warning backtrace

Part Number: TDA4AEN-Q1

Hi TI:

     I used the TDA4AEN J722S platform for my development. In each booting up, kernel have below case 1 and 2 warning backtrace. Could you please check how can I to fix this warning backtrace?

 

Below is my use yocto and RTOS SDK version information.

Linux yocto version: 10.01.00.04

MCU SDK RTOS version: sv_oz_tda4x_psdk_10_01_00_04_j722s

 

 

Case 1:

[   10.009955] Modules linked in: k3_j72xx_bandgap rti_wdt(+) cdns3_ti rtc_ti_k3 wave5 snd_soc_davinci_mcasp ti_k3_r5_remoteproc(+) snd_soc_ti_udma videobuf2_dma_contig videobuf2_memops sii902x(+) snd_soc_ti_edma v4l2_mem2mem videobuf2_v4l2 ds90ub953 ti_k3_dsp_remoteproc videobuf2_common sa2ul mcrc64 drm_kms_helper i2c_atr cfg80211 snd_soc_ti_sdma omap_hwspinlock omap_mailbox bluetooth ecdh_generic ecc rfkill cryptodev(O) fuse drm drm_panel_orientation_quirks backlight ipv6
[   10.010092] CPU: 3 PID: 200 Comm: (udev-worker) Tainted: G           O       6.6.44-ti-gee332fc84d96 #1
[   10.010104] Hardware name: Texas Instruments J722S EVM (DT)
[   10.010108] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   10.010117] pc : rti_wdt_probe+0x12c/0x5c0 [rti_wdt]
[   10.010146] lr : rti_wdt_probe+0x114/0x5c0 [rti_wdt]
[   10.010160] sp : ffff80008235b800
[   10.010163] x29: ffff80008235b850
[   10.015012] virtio_rpmsg_bus virtio4: creating channel ti.ipc4.ping-pong addr 0xe
[   10.015247] virtio_rpmsg_bus virtio4: msg received with no recipient
[   10.015691] virtio_rpmsg_bus virtio0: msg received with no recipient
[   10.016750] rproc-virtio rproc-virtio.5.auto: registered virtio4 (type 7)
[   10.016765] remoteproc remoteproc4: remote processor 78400000.r5f is now attached
[   10.022666]  x28: 0000000000000000 x27: 0000000000000000
[   10.022677] x26: ffff8000814bbb10 x25: ffff80008235bbb0 x24: 000000000000005b
[   10.022688] x23: ffff000820cb4c00 x22: ffff00082414ac90 x21: ffff000820cb4c10
[   10.022699] x20: ffff8000827ab090 x19: ffff00082414ac80 x18: ffffffffffffffff
[   10.022709] x17: 0000000000000000 x16: 0000000000000000 x15: ffff8000815db800
[   10.022718] x14: 0000000000000004 x13: 0000000000000290 x12: ffff8000827abfff
[   10.022728] x11: 0000000000002000 x10: ffff00097ffff010 x9 : 0000000000000100
[   10.022737] x8 : ffff8000827ab000 x7 : ffff00097ffff018 x6 : 00007fff8b945000
[   10.022747] x5 : 000000000e0f1000 x4 : ffff000820cb4e10 x3 : ffff0008250763c0
[   10.022757] x2 : ffff000825076480 x1 : ffff0008252cb900 x0 : ffff8000827ab000
[   10.022768] Call trace:
[   10.029967] virtio_rpmsg_bus virtio2: msg received with no recipient
[   10.036997]  rti_wdt_probe+0x12c/0x5c0 [rti_wdt]
[   10.037014]  platform_probe+0x68/0xc4
[   10.197149] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83TG721CS1.0] (irq=POLL)
[   10.200051]  really_probe+0x148/0x2b0
[   10.207194] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[   10.214286]  __driver_probe_device+0x78/0x12c
[   10.214297]  driver_probe_device+0xd8/0x15c
[   10.223530] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[   10.228525]  __driver_attach+0x90/0x19c
[   10.228540]  bus_for_each_dev+0x7c/0xdc
[   10.228549]  driver_attach+0x24/0x30
[   10.228557]  bus_add_driver+0xe4/0x208
[   10.228565]  driver_register+0x5c/0x124
[   10.228574]  __platform_driver_register+0x28/0x34
[   10.228581]  rti_wdt_driver_init+0x20/0x1000 [rti_wdt]
[   10.228596]  do_one_initcall+0x80/0x1c8
[   10.228605]  do_init_module+0x58/0x1e0
[   10.228617]  load_module+0x1c8c/0x1d18
[   10.338499]  init_module_from_file+0x88/0xcc
[   10.342775]  __arm64_sys_finit_module+0x1dc/0x2e4
[   10.347478]  invoke_syscall+0x48/0x114
[   10.351234]  el0_svc_common.constprop.0+0xc0/0xe0
[   10.355940]  do_el0_svc+0x1c/0x28
[   10.359251]  el0_svc+0x2c/0x84
[   10.362305]  el0t_64_sync_handler+0x120/0x12c
[   10.366655]  el0t_64_sync+0x190/0x194
[   10.370316] Code: b140041f 540010a8 91024014 a9096bf9 (b9400294)
[   10.376398] ---[ end trace 0000000000000000 ]---

 

 

Case 2:

[   10.513770] Internal error: synchronous external abort: 0000000096000010 [#2] PREEMPT SMP
[   10.523166] Modules linked in: pvrsrvkm(O+) e5010_jpeg_enc overlay crct10dif_ce v4l2_jpeg k3_j72xx_bandgap rti_wdt(+) cdns3_ti rtc_ti_k3 wave5 snd_soc_davinci_mcasp ti_k3_r5_remoteproc snd_soc_ti_udma videobuf2_dma_contig videobuf2_memops sii902x(+) snd_soc_ti_edma v4l2_mem2mem videobuf2_v4l2 ds90ub953 ti_k3_dsp_remoteproc videobuf2_common sa2ul mcrc64 drm_kms_helper i2c_atr cfg80211 snd_soc_ti_sdma omap_hwspinlock omap_mailbox bluetooth ecdh_generic ecc rfkill cryptodev(O) fuse drm drm_panel_orientation_quirks backlight ipv6
[   10.569812] CPU: 0 PID: 179 Comm: (udev-worker) Tainted: G      D    O       6.6.44-ti-gee332fc84d96 #1
[   10.569827] Hardware name: Texas Instruments J722S EVM (DT)
[   10.569832] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[   10.569840] pc : _RGXReadBVNCFromReg.isra.0+0x18/0x130 [pvrsrvkm]
[   10.597827] lr : RGXBvncInitialiseConfiguration+0x6d0/0x9d4 [pvrsrvkm]
[   10.603502] omap_i2c 20010000.i2c: controller timed out
[   10.604567] sp : ffff800081fab6a0
[   10.604570] x29: ffff800081fab6d0 x28: ffff80007999e064 x27: 0000000000000001
[   10.617280] sii902x: probe of 1-003b failed with error -110
[   10.620226] x26: ffff800081fab6a8 x25: ffff00082af4a160 x24: ffff800079971000
[   10.620239] x23: ffff000827b98308 x22: ffff00082af4a000 x21: ffff000827a0e008
[   10.640076] x20: ffff8000799b2458 x19: 0000000000000000 x18: 0000000000000000
[   10.640093] x17: ffff8008fdf7f000 x16: ffff800080000000 x15: 000000000d7841a0
[   10.640104] x14: 4954494e495f4345 x13: 0000000000000283 x12: 0000000000000002
[   10.640114] x11: ffff000827a0e008 x10: 0000000000000020 x9 : 0000000000000000
[   10.668605] x8 : 0000000000000024 x7 : ffff800083e80024 x6 : ffff800083e80000
[   10.675742] x5 : ffff800081fab6b0 x4 : ffff800081fab6ac x3 : ffff800081fab6a8
[   10.682877] x2 : ffff800081fab6a4 x1 : 0000000000000000 x0 : ffff000827a0e008
[   10.690010] Call trace:
[   10.692456]  _RGXReadBVNCFromReg.isra.0+0x18/0x130 [pvrsrvkm]
[   10.698452]  RGXRegisterDevice+0x400/0xb68 [pvrsrvkm]
[   10.703722]  PVRSRVCommonDeviceCreate+0x230/0x6ec [pvrsrvkm]
[   10.709600]  pvr_drm_load+0x98/0x1f0 [pvrsrvkm]
[   10.714371]  pvr_probe+0x60/0xac [pvrsrvkm]
[   10.718780]  platform_probe+0x68/0xc4
[   10.722451]  really_probe+0x148/0x2b0
[   10.726120]  __driver_probe_device+0x78/0x12c
[   10.730481]  driver_probe_device+0xd8/0x15c
[   10.734669]  __driver_attach+0x90/0x19c
[   10.738510]  bus_for_each_dev+0x7c/0xdc
[   10.742352]  driver_attach+0x24/0x30
[   10.745933]  bus_add_driver+0xe4/0x208
[   10.749687]  driver_register+0x5c/0x124
[   10.753531]  __platform_driver_register+0x28/0x34
[   10.758239]  pvr_init+0xb4/0x1000 [pvrsrvkm]
[   10.762731]  do_one_initcall+0x80/0x1c8
[   10.766575]  do_init_module+0x58/0x1e0
[   10.770334]  load_module+0x1c8c/0x1d18
[   10.774088]  init_module_from_file+0x88/0xcc
[   10.778364]  __arm64_sys_finit_module+0x1dc/0x2e4
[   10.783072]  invoke_syscall+0x48/0x114
[   10.786826]  el0_svc_common.constprop.0+0xc0/0xe0
[   10.791531]  do_el0_svc+0x1c/0x28
[   10.794849]  el0_svc+0x2c/0x84
[   10.797911]  el0t_64_sync_handler+0x120/0x12c
[   10.802269]  el0t_64_sync+0x190/0x194
[   10.805939] Code: 1100812a aa0003eb 91001148 8b0800c7 (b94000e7)
[   10.812028] ---[ end trace 0000000000000000 ]---

 

Below is attached log file:

booting_log_err_0205_v1.txt 

 

 

  • Hi,

    rti_wdt_probe

    Can you disable all the main_rti* nodes?

    arch/arm64/boot/dts/ti/k3-am62p-j722s-common-main.dtsi

    Seems like for some reason rti is crashing.

    pvr_drm_load

    Graphics is also crashing. Is this a custom board? Any changes that are done on top of SDK w.r.t graphics?

    - Keerthy

  • Hi Keerthy:

    Can you disable all the main_rti* nodes?

          --> If we disabled all of RTI watchdog function, does that's is ok? If our system happen hang, there have no watchdog to help us reboot system. Can you help us confirm that? Or the TDA4AEN J722S have no main_rti HW?

    Graphics is also crashing. Is this a custom board?

          ---> Yes, this is custom board. Not EVM board. 

    Any changes that are done on top of SDK w.r.t graphics?

    --> As I known that not change and graphics part. 

    Below my modify will remove the "Internal error: synchronous external abort pc : _RGXReadBVNCFromReg.isra.0+0x18/0x130 [pvrsrvkm]" backtrace.

    Simon

  • f we disabled all of RTI watchdog function, does that's is ok? If our system happen hang, there have no watchdog to help us reboot system. Can you help us confirm that? Or the TDA4AEN J722S have no main_rti HW?

    This is just to debug and go ahead. Please check and let me know if the hang is no longer there. I want to identify which instance is causing the crash.

    - Keerthy

  • Hi Keerthy:

    After modify below device tree to remove gpu and main_rti* node, I couldn't see those two warning kernel backtrace.

    k3-j722s-vision-apps.dtso: Remove the gpu and main_rti*

    /* Disable GPU for TDA4AEN-Q1 variant */
    &gpu {
        status = "disabled";
    };
    
    /* Disable RTI Watchdog that causes sync abort */
    &main_rti0 {
        status = "disabled";
    };
    
    &main_rti1 {
        status = "disabled";
    };
    
    &main_rti2 {
        status = "disabled";
    };
    
    &main_rti3 {
        status = "disabled";
    };
    
    &main_rti15 {
        status = "disabled";
    };

    kernel log remove gpu and main_rti* node:

    root@j722s-evm:~# dmesg
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 6.6.44-ti-gfbe7ed54d422 (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Fri Dec 26 02:58:02 UTC 2025
    [    0.000000] KASLR disabled due to lack of seed
    [    0.000000] Machine model: Texas Instruments J722S EVM
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] OF: reserved mem: 0x0000000080000000..0x000000008007ffff (512 KiB) nomap non-reusable tfa@80000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009e600000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node perception_buffer@9e600000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x000000009e600000..0x000000009e6fffff (1024 KiB) nomap non-reusable perception_buffer@9e600000
    [    0.000000] OF: reserved mem: 0x000000009e760000..0x000000009e77ffff (128 KiB) nomap non-reusable pstore@0x9e760000
    [    0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a00fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a0000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a0100000..0x00000000a0ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a0100000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a1000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a1100000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a2000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a3ffffff (31744 KiB) nomap non-reusable vision-apps-r5f-memory@a2100000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a5000000, size 32 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-rtos-ipc-memory-region@a5000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a5000000..0x00000000a6ffffff (32768 KiB) nomap non-reusable vision-apps-rtos-ipc-memory-region@a5000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 96 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@a7000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000a7000000..0x00000000acffffff (98304 KiB) nomap non-reusable vision-apps-dma-memory@a7000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ad000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@ad000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000ad000000..0x00000000ad0fffff (1024 KiB) nomap non-reusable vision-apps-c71-dma-memory@ad000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ad100000, size 63 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_0-memory@ad100000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000ad100000..0x00000000b0ffffff (64512 KiB) nomap non-reusable vision-apps-c71_0-memory@ad100000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b1000000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-dma-memory@b1000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000b1000000..0x00000000b10fffff (1024 KiB) nomap non-reusable vision-apps-c71_1-dma-memory@b1000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b1100000, size 63 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-c71_1-memory@b1100000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000b1100000..0x00000000b4ffffff (64512 KiB) nomap non-reusable vision-apps-c71_1-memory@b1100000
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000b5000000, size 40 MiB
    [    0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@b5000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x00000000b5000000..0x00000000b77fffff (40960 KiB) nomap non-reusable vision-apps-core-heap-memory-lo@b5000000
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 512 MiB
    [    0.000000] OF: reserved mem: initialized node c7x-ddr-heaps-hi@880000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x0000000880000000..0x000000089fffffff (524288 KiB) nomap non-reusable c7x-ddr-heaps-hi@880000000
    [    0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
    [    0.000000] OF: reserved mem: 0x0000000900000000..0x000000091fffffff (524288 KiB) map non-reusable vision_apps_shared-memories
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000980000000, size 896 MiB
    [    0.000000] OF: reserved mem: initialized node linux-cma-buffers@980000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: 0x0000000980000000..0x00000009b7ffffff (917504 KiB) map reusable linux-cma-buffers@980000000
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   [mem 0x0000000100000000-0x00000009ffffffff]
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x000000008007ffff]
    [    0.000000]   node   0: [mem 0x0000000080080000-0x000000009e5fffff]
    [    0.000000]   node   0: [mem 0x000000009e600000-0x000000009e6fffff]
    [    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e75ffff]
    [    0.000000]   node   0: [mem 0x000000009e760000-0x000000009e77ffff]
    [    0.000000]   node   0: [mem 0x000000009e780000-0x000000009e7fffff]
    [    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a3ffffff]
    [    0.000000]   node   0: [mem 0x00000000a4000000-0x00000000a4ffffff]
    [    0.000000]   node   0: [mem 0x00000000a5000000-0x00000000b77fffff]
    [    0.000000]   node   0: [mem 0x00000000b7800000-0x00000000ffffffff]
    [    0.000000]   node   0: [mem 0x0000000880000000-0x000000089fffffff]
    [    0.000000]   node   0: [mem 0x00000008a0000000-0x00000009ffffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000009ffffffff]
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.5
    [    0.000000] percpu: Embedded 20 pages/cpu s43176 r8192 d30552 u81920
    [    0.000000] pcpu-alloc: s43176 r8192 d30552 u81920 alloc=20*4096
    [    0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 root=PARTUUID=91352253-79f4-43a7-97a6-8bfa53276947 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 2064384
    [    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
    [    0.000000] software IO TLB: area num 4.
    [    0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
    [    0.000000] Memory: 5780984K/8388608K available (12736K kernel code, 1278K rwdata, 4324K rodata, 2560K init, 530K bss, 1690120K reserved, 917504K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
    [    0.000000]  Trampoline variant of Tasks RCU enabled.
    [    0.000000]  Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 256 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] Root IRQ handler: gic_handle_irq
    [    0.000000] GICv3: GICv3 features: 16 PPIs
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8a0800000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x00000008a0040000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008a0050000
    [    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008556] Console: colour dummy device 80x25
    [    0.013147] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.023815] pid_max: default: 32768 minimum: 301
    [    0.028614] LSM: initializing lsm=capability,selinux,integrity
    [    0.034596] SELinux:  Initializing.
    [    0.038288] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [    0.046046] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
    [    0.055943] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
    [    0.063243] RCU Tasks Trace: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
    [    0.071151] rcu: Hierarchical SRCU implementation.
    [    0.076050] rcu:     Max phase no-delay instances is 1000.
    [    0.081637] Platform MSI: msi-controller@1820000 domain created
    [    0.087957] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
    [    0.097417] EFI services will not be available.
    [    0.102318] smp: Bringing up secondary CPUs ...
    [    0.107553] Detected VIPT I-cache on CPU1
    [    0.107627] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
    [    0.107646] GICv3: CPU1: using allocated LPI pending table @0x00000008a0060000
    [    0.107696] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.108375] Detected VIPT I-cache on CPU2
    [    0.108431] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
    [    0.108445] GICv3: CPU2: using allocated LPI pending table @0x00000008a0070000
    [    0.108478] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.109071] Detected VIPT I-cache on CPU3
    [    0.109122] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
    [    0.109135] GICv3: CPU3: using allocated LPI pending table @0x00000008a0080000
    [    0.109166] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.109243] smp: Brought up 1 node, 4 CPUs
    [    0.188862] SMP: Total of 4 processors activated.
    [    0.193669] CPU features: detected: 32-bit EL0 Support
    [    0.198933] CPU features: detected: CRC32 instructions
    [    0.204240] CPU: All CPU(s) started at EL2
    [    0.208432] alternatives: applying system-wide alternatives
    [    0.215791] devtmpfs: initialized
    [    0.231061] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.241058] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
    [    0.272086] pinctrl core: initialized pinctrl subsystem
    [    0.277985] DMI not present or invalid.
    [    0.282525] NET: Registered PF_NETLINK/PF_ROUTE protocol family
    [    0.289483] DMA: preallocated 1024 KiB GFP_KERNEL pool for atomic allocations
    [    0.296920] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.305036] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.313281] audit: initializing netlink subsys (disabled)
    [    0.318987] audit: type=2000 audit(0.200:1): state=initialized audit_enabled=0 res=1
    [    0.319434] thermal_sys: Registered thermal governor 'step_wise'
    [    0.326909] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.333081] cpuidle: using governor menu
    [    0.343921] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.350931] ASID allocator initialised with 65536 entries
    [    0.357464] pstore: Using crash dump compression: deflate
    [    0.363001] printk: console [ramoops-1] enabled
    [    0.368146] pstore: Registered ramoops as persistent store backend
    [    0.374459] ramoops: using 0x20000@0x9e760000, ecc: 0
    [    0.394586] Modules: 27360 pages in range for non-PLT usage
    [    0.394603] Modules: 518880 pages in range for PLT usage
    [    0.401041] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.413434] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
    [    0.419838] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.426772] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
    [    0.433173] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.440107] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
    [    0.446510] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.453443] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
    [    0.461239] k3-chipinfo 43000014.chipid: Family:J722S rev:SR1.0 JTAGID[0x0bba002f] Detected
    [    0.470964] iommu: Default domain type: Translated
    [    0.475883] iommu: DMA domain TLB invalidation policy: strict mode
    [    0.482480] SCSI subsystem initialized
    [    0.486459] libata version 3.00 loaded.
    [    0.486629] usbcore: registered new interface driver usbfs
    [    0.492264] usbcore: registered new interface driver hub
    [    0.497720] usbcore: registered new device driver usb
    [    0.503368] mc: Linux media interface: v0.10
    [    0.507775] videodev: Linux video capture interface: v2.00
    [    0.513411] pps_core: LinuxPPS API ver. 1 registered
    [    0.518482] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.527824] PTP clock support registered
    [    0.531993] EDAC MC: Ver: 3.0.0
    [    0.535724] scmi_core: SCMI protocol bus registered
    [    0.541019] FPGA manager framework
    [    0.544598] Advanced Linux Sound Architecture Driver Initialized.
    [    0.551728] vgaarb: loaded
    [    0.554852] clocksource: Switched to clocksource arch_sys_counter
    [    0.561345] VFS: Disk quotas dquot_6.6.0
    [    0.565388] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.579120] Carveout Heap: Exported 512 MiB at 0x0000000900000000
    [    0.585476] NET: Registered PF_INET protocol family
    [    0.590753] IP idents hash table entries: 131072 (order: 8, 1048576 bytes, linear)
    [    0.603732] tcp_listen_portaddr_hash hash table entries: 4096 (order: 4, 65536 bytes, linear)
    [    0.612585] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
    [    0.620521] TCP established hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.629012] TCP bind hash table entries: 65536 (order: 9, 2097152 bytes, linear)
    [    0.638343] TCP: Hash tables configured (established 65536 bind 65536)
    [    0.645226] UDP hash table entries: 4096 (order: 5, 131072 bytes, linear)
    [    0.652328] UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes, linear)
    [    0.660003] NET: Registered PF_UNIX/PF_LOCAL protocol family
    [    0.666271] RPC: Registered named UNIX socket transport module.
    [    0.672349] RPC: Registered udp transport module.
    [    0.677155] RPC: Registered tcp transport module.
    [    0.681960] RPC: Registered tcp-with-tls transport module.
    [    0.687563] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.694149] NET: Registered PF_XDP protocol family
    [    0.699059] PCI: CLS 0 bytes, default 64
    [    0.704430] Initialise system trusted keyrings
    [    0.709213] workingset: timestamp_bits=46 max_order=21 bucket_order=0
    [    0.716119] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.722342] NFS: Registering the id_resolver key type
    [    0.727545] Key type id_resolver registered
    [    0.731821] Key type id_legacy registered
    [    0.735935] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.742784] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.782997] Key type asymmetric registered
    [    0.787199] Asymmetric key parser 'x509' registered
    [    0.792234] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
    [    0.799949] io scheduler mq-deadline registered
    [    0.804585] io scheduler kyber registered
    [    0.808714] io scheduler bfq registered
    [    0.815951] pinctrl-single 4084000.pinctrl: 34 pins, size 136
    [    0.822707] pinctrl-single f4000.pinctrl: 171 pins, size 684
    [    0.835271] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
    [    0.852539] loop: module loaded
    [    0.856772] megasas: 07.725.01.00-rc1
    [    0.864083] tun: Universal TUN/TAP device driver, 1.6
    [    0.869521] CAN device driver interface
    [    0.874349] VFIO - User Level meta-driver version: 0.3
    [    0.880706] usbcore: registered new interface driver usb-storage
    [    0.887435] i2c_dev: i2c /dev entries driver
    [    0.893135] sdhci: Secure Digital Host Controller Interface driver
    [    0.899476] sdhci: Copyright(c) Pierre Ossman
    [    0.904143] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.910526] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.916950] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    0.924171] usbcore: registered new interface driver usbhid
    [    0.929874] usbhid: USB HID core driver
    [    0.934338] mcur5f00_init: success to create /proc/mcu-r5f0-0_log
    [    0.941323] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
    [    0.950284] optee: probing for conduit method.
    [    0.954860] optee: revision 4.4 (8f645256efc0dc66)
    [    0.955173] optee: dynamic shared memory is enabled
    [    0.965772] random: crng init done
    [    0.969357] optee: initialized driver
    [    0.975062] Initializing XFRM netlink socket
    [    0.979483] NET: Registered PF_PACKET protocol family
    [    0.984650] can: controller area network core
    [    0.989139] NET: Registered PF_CAN protocol family
    [    0.994040] can: raw protocol
    [    0.997073] can: broadcast manager protocol
    [    1.001353] can: netlink gateway - max_hops=1
    [    1.005898] Key type dns_resolver registered
    [    1.018916] registered taskstats version 1
    [    1.023272] Loading compiled-in X.509 certificates
    [    1.040627] ti-sci 44043000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
    [    1.091385] omap_i2c 4900000.i2c: bus 2 rev0.12 at 400 kHz
    [    1.098099] omap_i2c 2b200000.i2c: bus 3 rev0.12 at 400 kHz
    [    1.104594] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
    [    1.111414] omap_i2c 20010000.i2c: bus 1 rev0.12 at 400 kHz
    [    1.117449] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
    [    1.125773] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
    [    1.134987] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
    [    1.143987] ti-sci-inta 4e400000.interrupt-controller: Interrupt Aggregator domain 200 created
    [    1.158272] ti-udma 485c0100.dma-controller: Number of rings: 82
    [    1.166809] ti-udma 485c0100.dma-controller: Channels: 44 (bchan: 16, tchan: 12, rchan: 16)
    [    1.177684] ti-udma 485c0000.dma-controller: Number of rings: 150
    [    1.188605] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
    [    1.198146] ti-udma 4e230000.dma-controller: Number of rings: 40
    [    1.207020] ti-udma 4e230000.dma-controller: Channels: 40 (bchan: 0, tchan: 8, rchan: 32)
    [    1.218219] printk: console [ttyS2] disabled
    [    1.222956] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 309, base_baud = 3000000) is a 8250
    [    1.231841] printk: console [ttyS2] enabled
    [    1.240316] printk: bootconsole [ns16550a0] disabled
    [    1.302842] davinci_mdio 8000f00.mdio: davinci mdio revision 17.7, bus freq 1000000
    [    1.572619] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83TG721CS1.0
    [    1.581370] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01903, cpsw version 0x6BA81903 Ports: 3 quirks:00000006
    [    1.594371] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
    [    1.601514] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
    [    1.608099] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010d, freq:500000000, add_val:1 pps:0
    [    1.622083] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
    [    1.632564] cpu cpu0: _of_add_opp_table_v2: no supported OPPs
    [    1.638426] cpu cpu0: OPP table can't be empty
    [    1.644251] mmc0: CQHCI version 5.10
    [    1.683404] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
    [    1.750495] mmc0: Command Queue Engine enabled
    [    1.754977] mmc0: new HS400 MMC card at address 0001
    [    1.760563] mmcblk0: mmc0:0001 AAM20E 29.6 GiB
    [    1.768906]  mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9
    [    1.774868] mmcblk0boot0: mmc0:0001 AAM20E 31.5 MiB
    [    1.780739] mmcblk0boot1: mmc0:0001 AAM20E 31.5 MiB
    [    1.786526] mmcblk0rpmb: mmc0:0001 AAM20E 4.00 MiB, chardev (238:0)
    [    2.698849] omap_i2c 20010000.i2c: controller timed out
    [    2.704105] ds90ub971 1-0018: Cannot read register 0x03: -110
    [    2.709925] ds90ub971: probe of 1-0018 failed with error -110
    [    2.721229] m_can_platform 20701000.can: m_can device registered (irq=519, version=32)
    [    2.730914] mmc1: CQHCI version 5.10
    [    2.735316] clk: Disabling unused clocks
    [    2.744186] ALSA device list:
    [    2.747244]   No soundcards found.
    [    2.771388] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
    [    2.902039] EXT4-fs (mmcblk0p5): mounted filesystem 2ec70be8-8f8f-4121-ac64-446675477f10 r/w with ordered data mode. Quota mode: none.
    [    2.914296] VFS: Mounted root (ext4 filesystem) on device 179:5.
    [    2.921256] devtmpfs: mounted
    [    2.925011] Freeing unused kernel memory: 2560K
    [    2.929644] Run /sbin/init as init process
    [    2.933742]   with arguments:
    [    2.933746]     /sbin/init
    [    2.933750]   with environment:
    [    2.933753]     HOME=/
    [    2.933758]     TERM=linux
    [    3.017031] mmc1: new ultra high speed SDR104 SDXC card at address aaaa
    [    3.024431] mmcblk1: mmc1:aaaa SN128 119 GiB
    [    3.034114]  mmcblk1: p1
    [    3.034489] systemd[1]: System time before build time, advancing clock.
    [    3.066060] NET: Registered PF_INET6 protocol family
    [    3.072069] Segment Routing with IPv6
    [    3.075791] In-situ OAM (IOAM) with IPv6
    [    3.103521] systemd[1]: systemd 255.13^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified)
    [    3.135455] systemd[1]: Detected architecture arm64.
    [    3.155923] systemd[1]: Hostname set to <j722s-evm>.
    [    3.164243] systemd[1]: Initializing machine ID from random generator.
    [    3.457584] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.566065] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.657118] systemd[1]: Queued start job for default target Graphical Interface.
    [    3.693287] systemd[1]: Created slice Slice /system/getty.
    [    3.717505] systemd[1]: Created slice Slice /system/modprobe.
    [    3.741422] systemd[1]: Created slice Slice /system/serial-getty.
    [    3.764805] systemd[1]: Created slice User and Session Slice.
    [    3.787342] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [    3.811224] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [    3.835029] systemd[1]: Expecting device /dev/disk/by-partlabel/persist...
    [    3.858943] systemd[1]: Expecting device /dev/disk/by-partlabel/userdata...
    [    3.882920] systemd[1]: Expecting device /dev/ttyS2...
    [    3.899104] systemd[1]: Reached target Path Units.
    [    3.918977] systemd[1]: Reached target Remote File Systems.
    [    3.938978] systemd[1]: Reached target Slice Units.
    [    3.954980] systemd[1]: Reached target Swaps.
    [    4.009054] systemd[1]: Listening on RPCbind Server Activation Socket.
    [    4.031134] systemd[1]: Reached target RPC Port Mapper.
    [    4.058577] systemd[1]: Listening on Process Core Dump Socket.
    [    4.079710] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [    4.104359] systemd[1]: Listening on Journal Audit Socket.
    [    4.127746] systemd[1]: Listening on Journal Socket (/dev/log).
    [    4.151777] systemd[1]: Listening on Journal Socket.
    [    4.171894] systemd[1]: Listening on Network Service Netlink Socket.
    [    4.197880] systemd[1]: Listening on udev Control Socket.
    [    4.219624] systemd[1]: Listening on udev Kernel Socket.
    [    4.239641] systemd[1]: Listening on User Database Manager Socket.
    [    4.291239] systemd[1]: Mounting Huge Pages File System...
    [    4.311456] systemd[1]: Mounting POSIX Message Queue File System...
    [    4.339214] systemd[1]: Mounting /sys/fs/pstore...
    [    4.363675] systemd[1]: Mounting Kernel Debug File System...
    [    4.383595] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
    [    4.402115] systemd[1]: Mounting Temporary Directory /tmp...
    [    4.425313] systemd[1]: Starting Create List of Static Device Nodes...
    [    4.452099] systemd[1]: Starting Load Kernel Module configfs...
    [    4.472151] systemd[1]: Starting Load Kernel Module drm...
    [    4.492095] systemd[1]: Starting Load Kernel Module fuse...
    [    4.517963] systemd[1]: Starting Start psplash boot splash screen...
    [    4.527709] fuse: init (API version 7.39)
    [    4.578968] systemd[1]: Starting RPC Bind...
    [    4.599393] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
    [    4.620584] systemd[1]: Starting Journal Service...
    [    4.646249] systemd[1]: Starting Load Kernel Modules...
    [    4.668867] systemd[1]: Starting Generate network units from Kernel command line...
    [    4.687812] cryptodev: loading out-of-tree module taints kernel.
    [    4.698414] cryptodev: driver 1.14 loaded.
    [    4.723979] systemd[1]: Starting Remount Root and Kernel File Systems...
    [    4.724537] systemd-journald[122]: Collecting audit messages is enabled.
    [    4.761518] systemd[1]: Starting Coldplug All udev Devices...
    [    4.787611] EXT4-fs (mmcblk0p5): re-mounted 2ec70be8-8f8f-4121-ac64-446675477f10 r/w. Quota mode: none.
    [    4.793398] systemd[1]: Started RPC Bind.
    [    4.813546] systemd[1]: Started Journal Service.
    [    5.246513] systemd-journald[122]: Received client request to flush runtime journal.
    [    5.459313] audit: type=1334 audit(1728487094.424:2): prog-id=6 op=LOAD
    [    5.466102] audit: type=1334 audit(1728487094.428:3): prog-id=7 op=LOAD
    [    5.472767] audit: type=1334 audit(1728487094.436:4): prog-id=8 op=LOAD
    [    5.809872] audit: type=1334 audit(1728487094.772:5): prog-id=9 op=LOAD
    [    5.816678] audit: type=1334 audit(1728487094.780:6): prog-id=10 op=LOAD
    [    6.080137] audit: type=1334 audit(1728487095.044:7): prog-id=11 op=LOAD
    [    6.107650] audit: type=1334 audit(1728487095.072:8): prog-id=12 op=LOAD
    [    6.486396] m_can_platform 20701000.can main_mcan0: renamed from can0
    [    7.553879] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fca100
    [    7.598998] audit: type=1334 audit(1728487096.560:9): prog-id=13 op=LOAD
    [    7.605862] omap-mailbox 29010000.mailbox: omap mailbox rev 0x66fca100
    [    7.651258] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fca100
    [    7.658939] omap-mailbox 29030000.mailbox: omap mailbox rev 0x66fca100
    [    7.690003] k3-dsp-rproc 7e000000.dsp: assigned reserved memory node vision-apps-c71-dma-memory@ad000000
    [    7.701986] k3-dsp-rproc 7e000000.dsp: configured DSP for IPC-only mode
    [    7.752483] remoteproc remoteproc0: 7e000000.dsp is available
    [    7.758485] remoteproc remoteproc0: attaching to 7e000000.dsp
    [    7.793510] rproc-virtio rproc-virtio.0.auto: assigned reserved memory node vision-apps-c71-dma-memory@ad000000
    [    7.805531] virtio_rpmsg_bus virtio0: rpmsg host is online
    [    7.808730] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
    [    7.810112] platform 79000000.r5f: configured R5F for IPC-only mode
    [    7.810276] platform 79000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a1000000
    [    7.811115] remoteproc remoteproc1: 79000000.r5f is available
    [    7.819691] rproc-virtio rproc-virtio.0.auto: registered virtio0 (type 7)
    [    7.824538] remoteproc remoteproc1: attaching to 79000000.r5f
    [    7.833595] remoteproc remoteproc0: remote processor 7e000000.dsp is now attached
    [    7.848560] k3-dsp-rproc 7e200000.dsp: assigned reserved memory node vision-apps-c71_1-dma-memory@b1000000
    [    7.858017] rproc-virtio rproc-virtio.1.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a1000000
    [    7.860817] k3-dsp-rproc 7e200000.dsp: configured DSP for IPC-only mode
    [    7.871270] rtc-ti-k3 2b1f0000.rtc: registered as rtc0
    [    7.880794] remoteproc remoteproc2: 7e200000.dsp is available
    [    7.881706] virtio_rpmsg_bus virtio1: rpmsg host is online
    [    7.881741] rproc-virtio rproc-virtio.1.auto: registered virtio1 (type 7)
    [    7.881750] remoteproc remoteproc1: remote processor 79000000.r5f is now attached
    [    7.886115] rtc-ti-k3 2b1f0000.rtc: setting system clock to 1970-01-01T00:00:00 UTC (0)
    [    7.891433] remoteproc remoteproc2: attaching to 7e200000.dsp
    [    7.902334] vdec 30210000.video-codec: OPP table not found in device tree
    [    7.929049] ds90ub953 1-0018: error -ENODEV: Platform data missing
    [    7.931290] rproc-virtio rproc-virtio.3.auto: assigned reserved memory node vision-apps-c71_1-dma-memory@b1000000
    [    7.931356] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
    [    7.931954] platform 78000000.r5f: configured R5F for IPC-only mode
    [    7.932098] platform 78000000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
    [    7.932877] remoteproc remoteproc3: 78000000.r5f is available
    [    7.932978] remoteproc remoteproc3: attaching to 78000000.r5f
    [    7.933324] rproc-virtio rproc-virtio.4.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a0000000
    [    7.933785] virtio_rpmsg_bus virtio2: rpmsg host is online
    [    7.933810] rproc-virtio rproc-virtio.4.auto: registered virtio2 (type 7)
    [    7.933816] remoteproc remoteproc3: remote processor 78000000.r5f is now attached
    [    7.937602] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xd
    [    7.948573] sii902x 1-003b: supply iovcc not found, using dummy regulator
    [    7.955197] platform 78400000.r5f: configured R5F for IPC-only mode
    [    7.957032] virtio_rpmsg_bus virtio3: rpmsg host is online
    [    7.957068] rproc-virtio rproc-virtio.3.auto: registered virtio3 (type 7)
    [    7.957075] remoteproc remoteproc2: remote processor 7e200000.dsp is now attached
    [    7.966679] sii902x 1-003b: supply cvcc12 not found, using dummy regulator
    [    7.973051] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0xd
    [    7.974506] platform 78400000.r5f: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
    [    8.033359] vdec 30210000.video-codec: Added wave5 driver with caps: 'ENCODE' 'DECODE'
    [    8.044773] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xe
    [    8.049815] vdec 30210000.video-codec: Product Code:      0x521c
    [    8.109862] vdec 30210000.video-codec: Firmware Revision: 334314
    [    8.122699] remoteproc remoteproc4: 78400000.r5f is available
    [    8.128900] remoteproc remoteproc4: attaching to 78400000.r5f
    [    8.173905] dbus-broker-lau[537]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set
    [    8.202012] rproc-virtio rproc-virtio.5.auto: assigned reserved memory node vision-apps-r5f-dma-memory@a2000000
    [    8.229128] virtio_rpmsg_bus virtio4: rpmsg host is online
    [    8.231683] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0xd
    [    8.237144] rproc-virtio rproc-virtio.5.auto: registered virtio4 (type 7)
    [    8.242498] virtio_rpmsg_bus virtio4: creating channel rpmsg_chrdev addr 0x15
    [    8.256441] virtio_rpmsg_bus virtio4: creating channel ti.ipc4.ping-pong addr 0xe
    [    8.264262] virtio_rpmsg_bus virtio4: msg received with no recipient
    [    8.267745] remoteproc remoteproc4: remote processor 78400000.r5f is now attached
    [    8.270707] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15
    [    8.285791] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xe
    [    8.299122] virtio_rpmsg_bus virtio0: msg received with no recipient
    [    8.305702] virtio_rpmsg_bus virtio3: creating channel rpmsg_chrdev addr 0x15
    [    8.313115] virtio_rpmsg_bus virtio3: creating channel ti.ipc4.ping-pong addr 0xe
    [    8.321022] virtio_rpmsg_bus virtio3: msg received with no recipient
    [    8.323010] e5010 fd20000.e5010: Device registered as /dev/video2
    [    8.561810] audit: type=1334 audit(1728487097.523:10): prog-id=14 op=LOAD
    [    8.572720] audit: type=1334 audit(1728487097.531:11): prog-id=15 op=LOAD
    [    8.753720] Bluetooth: Core ver 2.22
    [    8.759098] NET: Registered PF_BLUETOOTH protocol family
    [    8.766920] Bluetooth: HCI device and connection manager initialized
    [    8.773381] Bluetooth: HCI socket layer initialized
    [    8.779051] Bluetooth: L2CAP socket layer initialized
    [    8.786963] Bluetooth: SCO socket layer initialized
    [    9.066923] omap_i2c 20010000.i2c: controller timed out
    [    9.142933] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    9.146591] sii902x: probe of 1-003b failed with error -110
    [    9.171436] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x14
    [    9.171655] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x15
    [    9.171762] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x28
    [    9.171857] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x29
    [    9.171939] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x2a
    [    9.172026] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0x2b
    [    9.172244] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    9.173073] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
    [    9.559628] xhci-hcd xhci-hcd.6.auto: xHCI Host Controller
    [    9.565428] xhci-hcd xhci-hcd.6.auto: new USB bus registered, assigned bus number 1
    [    9.588267] xhci-hcd xhci-hcd.6.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000008010
    [    9.598167] xhci-hcd xhci-hcd.6.auto: irq 537, io mem 0x31210000
    [    9.608593] xhci-hcd xhci-hcd.6.auto: xHCI Host Controller
    [    9.615137] xhci-hcd xhci-hcd.6.auto: new USB bus registered, assigned bus number 2
    [    9.655085] xhci-hcd xhci-hcd.6.auto: Host supports USB 3.0 SuperSpeed
    [    9.711475] hub 1-0:1.0: USB hub found
    [    9.717395] hub 1-0:1.0: 1 port detected
    [    9.806975] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
    [    9.855433] hub 2-0:1.0: USB hub found
    [    9.886147] hub 2-0:1.0: 1 port detected
    [   10.002331] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83TG721CS1.0] (irq=POLL)
    [   10.012500] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
    [   10.718518] EXT4-fs (mmcblk0p9): recovery complete
    [   10.740960] EXT4-fs (mmcblk0p9): mounted filesystem e57a23c2-fa6d-11f0-8c7f-7f0c16c33f26 r/w with ordered data mode. Quota mode: none.
    [   11.140733] EXT4-fs (mmcblk0p2): recovery complete
    [   11.146287] EXT4-fs (mmcblk0p2): mounted filesystem e551114e-fa6d-11f0-a367-6763d0905145 r/w with ordered data mode. Quota mode: none.
    [   11.147726] kauditd_printk_skb: 2 callbacks suppressed
    [   11.147742] audit: type=1701 audit(1728487100.111:14): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=876 comm="dlt-system" exe="/usr/bin/dlt-system" sig=11 res=1
    [   11.217178] audit: type=1006 audit(1728487100.179:15): pid=878 uid=0 subj=kernel old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
    [   11.233801] audit: type=1300 audit(1728487100.179:15): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=ffffe1977c38 a2=4 a3=1 items=0 ppid=1 pid=878 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
    [   11.262221] audit: type=1327 audit(1728487100.179:15): proctitle="(systemd)"
    [   11.514914] audit: type=1701 audit(1728487100.475:16): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=904 comm="dlt-system" exe="/usr/bin/dlt-system" sig=11 res=1
    [   11.853362] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83TG721CS1.0] (irq=POLL)
    [   11.890684] audit: type=1701 audit(1728487100.851:17): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=936 comm="dlt-system" exe="/usr/bin/dlt-system" sig=11 res=1
    [   11.893096] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
    [   12.204834] audit: type=1701 audit(1728487101.167:18): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=962 comm="dlt-system" exe="/usr/bin/dlt-system" sig=11 res=1
    [   12.627542] audit: type=1006 audit(1728487101.591:19): pid=787 uid=0 subj=kernel old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1
    [   12.641403] audit: type=1300 audit(1728487101.591:19): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=fffff5fdc6d8 a2=4 a3=1 items=0 ppid=1 pid=787 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
    [   12.669116] audit: type=1327 audit(1728487101.591:19): proctitle="(weston)"
    [   20.108396] platform 4e08000.can: deferred probe pending
    [   20.113923] platform 4e18000.can: deferred probe pending
    [   76.428856] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
    root@j722s-evm:~#
    

  • Thanks for the confirmation. Now let us tackle watchdog first.

    Can you isolate if one particular instance of main_rti causes this issue or any of them causes?

    Based on that we can disable a particular one and rest can work. For GPU I will loop in expert once we are through the RTI issue.

    - Keerty

  • Hi Keerty:

    Can you isolate if one particular instance of main_rti causes this issue or any of them causes?

          After check the device disabled the main_rti 15 would have remove the warning kernel backtrace. 

    Based on that we can disable a particular one and rest can work. For GPU I will loop in expert once we are through the RTI issue.

           Please help check with GPU and RTI expert for this kernel warning backtrace problem. Do we need to disable the gpu and main_rti_15 to fix this warning backtrace? Thanks, your help

    Simon

  • Hi Simon,

    Thanks for isolating that. Since other watchdogs are functional. Please disable this instance.

    I am looping in our GPU expert on the other crash.

    Best Regards,

    Keerthy

  • Hi Keerthy:

          I have question that why the TDA4AEN have need to disable the RTI_15. I have also check the TDAM J722S EVM platfrom kernel log. But I didn't find those warning backtrace. So if I disabled the RTI_15 would be fine? Have no any problme?

    Br,

    Simon

  • Please help check with GPU and RTI expert for this kernel warning backtrace problem. Do we need to disable the gpu and main_rti_15 to fix this warning backtrace? Thanks, your help

    If you enable the GPU and keep rti_15 disabled, are you able to run 'pvrlogdump and capture any logs?'

    If not, can you blacklist GPU following the instructions here:  [FAQ] How do I disable the GPU driver from loading? 

    You should then load driver manually and log any crashes or run 'pvrlogdump'

    Thanks,
    Sarabesh S.

  • Hi Sarabesh:

    Without disable gpu and any rti_*. I run the prvlogdump and shown as below log. 

    root@j722s-evm:/tmp# pvrlogdump
    Checking driver state ............... initialised
    Checking for debugfs ................ found
    Checking for lockdep ................ not found
    Checking for ftrace ................. not found
    Checking for firmware log groups .... not found
    There are no AppHints enabled in /etc/powervr.ini or in debugfs
    for any of the firmware log groups. Unless 'pvrdebug' tool
    was used for that purpose there will be no information in
    firmware log.
    Please consider enabling some of the firmware log groups
    before the problem occurs.

    Dumping data ........................ done
    Archiving data ...................... done

    File /tmp/pvrlogdump_j722s-evm_2410091857.txt.gz was created.

    I also find the kernel log show as below fail log.

    j722s-evm login: [   21.672164] platform 4e18000.can: deferred probe pending
    [   21.677524] platform 4e08000.can: deferred probe pending
    [ 1470.770000]
    [ 1470.771720] ==== debug_dump (gpu00, 1) ====
    [ 1470.776078]
    [ 1470.796925] pvrdebug failed
    [ 1470.836346]
    [ 1470.837936] ==== debug_dump (gpu00, 2) ====
    [ 1470.842266]
    [ 1470.851859] pvrdebug failed
    [ 1470.962245] PVR_K:(Error): 10108: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (73) [687]
    [ 1470.975367] PVR_K:(Error): 10109: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (72) [687]
    [ 1470.988425] PVR_K:(Error): 10110: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (71) [687]
    [ 1471.001574] PVR_K:(Error): 10111: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (70) [687]
    [ 1471.014557] PVR_K:(Error): 10112: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (69) [687]
    [ 1471.027626] PVR_K:(Error): 10113: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (68) [687]
    [ 1471.040604] PVR_K:(Error): 10114: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (67) [687]
    [ 1471.053742] PVR_K:(Error): 10115: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (66) [687]
    [ 1473.139305]
    [ 1473.140895] ==== debug_dump (gpu00, 1) ====
    [ 1473.145230]
    [ 1473.155026] pvrdebug failed
    [ 1473.192691]
    [ 1473.194278] ==== debug_dump (gpu00, 2) ====
    [ 1473.198591]
    [ 1473.208146] pvrdebug failed
    [ 1495.400235]
    [ 1495.401827] ==== debug_dump (gpu00, 1) ====
    [ 1495.406215]
    [ 1495.416088] pvrdebug failed
    [ 1495.453930]
    [ 1495.455653] ==== debug_dump (gpu00, 2) ====
    [ 1495.459948]
    [ 1495.469334] pvrdebug failed
    [ 1495.586869] PVR_K:(Error): 10324: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (73) [687]
    [ 1495.600833] PVR_K:(Error): 10325: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (72) [687]
    [ 1495.613989] PVR_K:(Error): 10326: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (71) [687]
    [ 1495.626999] PVR_K:(Error): 10327: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (70) [687]
    [ 1495.640803] PVR_K:(Error): 10328: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (69) [687]
    [ 1495.654201] PVR_K:(Error): 10329: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (68) [687]
    [ 1495.668136] PVR_K:(Error): 10330: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (67) [687]
    [ 1495.682220] PVR_K:(Error): 10331: Uninitialised AppHint device for AppHint in                                                                                                                                                             dex (66) [687]
    [ 1497.768214]
    [ 1497.769804] ==== debug_dump (gpu00, 1) ====
    [ 1497.774219]
    [ 1497.783911] pvrdebug failed
    [ 1497.823416]
    [ 1497.825062] ==== debug_dump (gpu00, 2) ====
    [ 1497.829445]
    [ 1497.839028] pvrdebug failed
    

    Attach the dump log file:

    pvrlogdump_j722s-evm_2410091857.txt.gz

  • Hi Sarabesh:

           One more question that TDA4AEN platform have GPU HW or not?

    Br,

    Simon

  •        One more question that TDA4AEN platform have GPU HW or not?

    The TDA4AEN does not have a GPU, it is the TDA4VEN that has a GPU. You can refer to the datasheet which has a table stating the differences between VEN and AEN starting on page 6.

    Could you try to replicate this on an J722s EVM?

    Thanks,
    Sarabesh S.

  • Hi Sarabesh:

          I confirm that before. I have test on my J722S EVM and no see the gpu warning backtrace.

    Br,

    Simon

  • Hi Simon,

    I will share the logs with our IP Vendor and let you know their feedback. To be clear is this happening on boot or upon running an GPU application?

    Regards,
    Sarabesh S.

  • Hi Sarabesh:

          This is happening on the booting up log only!

    Br,

    Simon

  • Hi Simon, 

    Thanks for the clarification. I will follow up with our IP vendor and let you know. 

    Regards,
    Sarabesh S.

  • Simon, 

    Could you clarify a some more points for me: 

    What is the result when disabling only main_rti15? Are you able to run any out-of-box GPU demos (i.e. kmscube, glmark2, rgxcompute) or does the GPU still fail on boot?

    Are you able to run pvrdebug -loggroups main,mts,hwr?

    Thanks,
    Sarabesh S.

  • Hi Sarabesh:

          How can I to doing the any test when I only disable the main_rti15? Can you tell me what command I can doing test. Because I's not know how to test GPU function. Thanks, your help!

    Br,

    Simon

  • Hi Simon, 

    If you're not able to run simple out-of-box demo's like rgx_compute_test or see an error then GPU is not working.

    Are you able to run pvrdebug -loggroups main,mts,hwr?

    Let me know if you can share this.

    Regards,
    Sarabesh S.

  • Hi Sarabesh:

          I want confirm two item:

             1. In the TDA4AEN no GPU HW. So we will disable the GPU in kernel device tree. Is it seem that ok? Because there have no GPU HW.

             2. In the TDA4AEN, can I disable the main_rti15 watchdog? If we disable have any effect? 

  • Hi Simon, 

    1. There is no problem disabling GPU in device tree since you have no use for the GPU.

    2. I will let  respond to this. 

    Regards,
    Sarabesh S.

  • Yes no issues with disabling that instance of RTI.

    Closing this thread. 

    Best Regards,

    Keerthy