This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

arago streamer-ti v4lsrc on DM365

I'm trying to build gstreamer-ti to use ipipe management of dm365 (really I'm using a board based on dm365).

I'm starting to build from overlays:

  • arago: modified from arago main line branch master HASH dfacf37be96127b8613456105b70e43e1fdb4af1
  • arago-oe-dev:  modified from main line branch master HASH 0e80c2e667e6eabffa69fc069376695baabeb4c3

but no modifications in "arago/recipes/ti"  are been made.

The building go to the and without problems, but no texas customization or patch are applied (this is ipipe management), in fact when I use this pipeline from device:

gst-launch v4l2src always-copy=FALSE ! 'video/x-raw-yuv,format=(fourcc)NV12,width=1280,height=720,framerate=(fraction)30/1' !  TIVidenc1 bitRate=3000000 encodingPreset=2 codecName=h264enc engineName=codecServer contiguousInputFrame=TRUE ! rtph264pay pt=96 ! udpsink host=192.168.1.107 port=5000

it dosen't work.

Supporting to this test, I stop the gstremer-ti building entering into devshell mode before do_configure and do_compile steps, and run these two manually.

Into the package dowloaded from SRC_URI in the related recipe there are:

  • source tarball of gstreamer and four gst-plugins
  • texas patches divided by related source

I see that during compilation no sources tarball are untar, and no patches are applied for ipipe management.

I'ts one month thst i try to solve this question

Tnx in advance for any help

Damiano