Part Number: SK-AM62A-LP
Hello,
I'm working on reducing boot time for an AM62A design based on the tisdk-tiny-sdk, booting from an SD card. I am working in Yocto, using an SPL boot flow. Adding:
--- a/board/ti/am62ax/am62ax.env
+++ b/board/ti/am62ax/am62ax.env
@@ -11,7 +11,7 @@ rproc_fw_binaries= 0 /lib/firmware/am62-mcu-m4f0_0-fw
name_kern=Image
console=ttyS2,115200n8
-args_all=setenv optargs ${optargs} earlycon=ns16550a,mmio32,0x02800000
+args_all=setenv optargs ${optargs} earlycon=ns16550a,mmio32,0x02800000 loglevel=1
${mtdparts}
run_kern=booti ${loadaddr} ${rd_spec} ${fdtaddr}
also reduces boot time by about 5sec, but does not work while in Falcon mode. I understand that U-boot is skipped in Falcon mode, so this is not a surprise, but adding bootargs to the dts does not work in either a standard boot flow or Falcon mode.
--- a/arch/arm64/boot/dts/ti/k3-am62a7-sk.dts
+++ b/arch/arm64/boot/dts/ti/k3-am62a7-sk.dts
@@ -33,6 +33,7 @@
chosen {
stdout-path = "serial2:115200n8";
+ bootargs = "console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 loglevel=1";
};
memory@80000000 {
I also tried adding:
Can you please advise on how I can suppress kernel prints during boot while in Falcon mode?