Booting Linux the Micron SSD SATA drive does not connect to the AM3892 Processor. After hooking up a SATA analyser it turns out that the Host is only sending ALIGN commands to the drive. I would have expect some SYNC primitives. Does the SATA controller follow the SATA spec and if so, what version? If not, can you highlight the differences between the two for us?
-mike