This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel Panic while playing 720P Video on OMAP37xx

Other Parts Discussed in Thread: OMAP3530

On OMAP37xx EVM with External 10" LCD (1360x768) running at Legacy Mode.

Condition 1:

After playing the 720P MAPG-4 Video, which comes with EVM SDCard, for 1 or 2 mins and then kernel panic occurs. Any optimization is needed on kernel param??

Internal error: Oops - undefined instruction: 0 [#1]
last sysfs file: /sys/devices/system/cpu/cpu0/cpufreq/stats/time_in_state
Modules linked in: omaplfb pvrsrvkm sdmak lpm_omap3530 dsplinkk cmemk                                        
CPU: 0    Not tainted  (2.6.32 #34)                                                                             
PC is at unmap_vmas +0x334/0x574
LR is at unmap_vmas +0x334/0x574
pc : [<c00a5dbc>]    lr : [<c00a5dbc>]    psr: 20000013
sp : c4991ea0  ip : 00000000  fp : c1ce6c18
r10: 003e1fbb  r9 : afd40000  r8 : 00000000
r7 : c82385f8  r6 : c05203ac  r5 : c0786780  r4 : afd06000
r3 : c0786788  r2 : ffffffff  r1 : 00000018  r0 : c0786780
Flags: nzCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user
Control: 10c5387d  Table: 88fe4019  DAC: 00000015

Before the kernel panic, the video on the 10" External LCD freeze and only sound was coming. With-in next 1 min, kernel panic occured.

Condition 2:

No Kernel panic. But video stopped. Gallary Not responding:

 W/AudioFlinger( 1867): write blocked for 354 msecs, 1 delayed writes, thread 0x38a70
D/TIOverlay( 1493): overlay_createOverlay:IN w=1280 h=544 format=0x16
I/Overlay ( 1493): v4l2_overlay_init:: w=1280 h=544
I/Overlay ( 1493): v4l2_overlay_init:: w=1280 h=544
I/Overlay ( 1493): v4l2_overlay_init:: w=1280 h=544
I/Overlay ( 1493): 3 buffers allocated 3 requested
I/Overlay ( 1493): buffer cookie is 2
D/TIOverlay( 1493): found display 0 [lcd] enabled
I/TIOverlay( 1493): Opened video1/fd=178/obj=00208850/shm=177/size=4096
D/TIOverlay( 1493): overlay_createOverlay: OUT
I/TIOverlay( 1867): Postponing Stream Enable/0/1
I/TIOverlay( 1493): Position/X0/Y0/W0/H0
I/TIOverlay( 1493): Adjusted Position/X0/Y95/W1360/H578
I/TIOverlay( 1493): Rotation/0
I/Overlay ( 1493): v4l2_overlay_set_position:: original w=728 h=544
I/Overlay ( 1493): v4l2_overlay_set_position:: new w=1360 h=578
I/Overlay ( 1493): dumping driver state:
I/Overlay ( 1493): output pixfmt: w 1280, h 544, colorsapce 7, pixfmt UYVY
I/Overlay ( 1493): v4l2_overlay window: l 0, t 95, w 1360, h 578
I/Overlay ( 1493): output crop: l 0, t 0, w 1280, h 544
I/TIOverlay( 1867): Queue more buffers before attempting to dequeue
I/CacheService( 1770): Preparing DiskCache for all thumbnails.
I/CacheService( 1770): DiskCache ready for all thumbnails.
W/InputManagerService( 1493): Window already focused, ignoring focus gain of: com.android.internal.view.IInputMethodClient$Stub$Proxy@4082a078
D/dalvikvm( 1650): GC_EXPLICIT freed 326K, 53% free 2680K/5639K, external 716K/1038K, paused 31ms
W/KeyCharacterMap( 1770): No keyboard for id 65536
W/KeyCharacterMap( 1770): Using default keymap: /system/usr/keychars/qwerty.kcm.bin
W/ActivityManager( 1493): Activity pause timeout for HistoryRecord{4075dcc0 com.cooliris.media/.MovieView}
I/InputDispatcher( 1493): Application is not responding: AppWindowToken{407992c0 token=HistoryRecord{407983f8 com.cooliris.media/.Gallery}}.  5004.5ms since event, 5004.4ms sind
I/WindowManager( 1493): Input event dispatching timed out sending to application AppWindowToken{407992c0 token=HistoryRecord{407983f8 com.cooliris.media/.Gallery}}
I/Process ( 1493): Sending signal. PID: 1770 SIG: 3