This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High Speed DSS OMAP37xx

Currently my 10" LG Laptop 18bit LCD (1360x768) is connected to DSS thru LVDS converter, in legacy mode (PCLK < 60MHz). The LCD need minimum of 66MHz PCLK (High Speed). But it is working in Legacy mode.

My doubts are:

1. Running the LCD at Legacy mode will affect the 720P playback?

2. To run the 18bit LCD at high speed, only pin mux changes are enough and no need to touch the sysboot pins? (Ref: http://processors.wiki.ti.com/index.php/OMAP35x_To_AM37x_Hardware_Migration_Guide#Pinmultiplexing_updates)

3. How to check/enable the Dithering mode?